Skip to main content
md1
Associate III
Aug 27, 2004 5:23 AM UTC
Question

Development Tools

Posted on August 27, 2004 at 07:23

Development Tools

This topic has been closed for replies.

3 replies

md1
md1Author
Associate III
Aug 12, 2004 7:16 AM UTC
Posted on August 12, 2004 at 09:16

Hello,

I am a little confused over the ordering codes for the ST7MDT20-DVP3 and ST7MDT10-DVP3.

As far as I can see, if I order an ST7MDT20-DVP, According to the user manual I will get the following:

A base MEB, a TEB for the 521/321, and an SDIP32 and SDIP42 connectors.

So if I wanted to work with the TQFP64 (14x14) then in addition to ordering the ST7MDT20-DVP3 I would have to order the ST7MDT20-T64/DVP also.

Now, I also want to work with the FLITE devices as well. So I now will order a TEB for my FLITE, because I already have an MEB from the ST7MDT20-DVP. So I will order an additional ST7MDT10-TEB/DVP. My first question is will I get a default DIP16/SO16 kit with the TEB, or will I have to order this seperately? (ST7MDT10-16/DVP).

My other issue is that in the user guide for the ST7MDT10-DVP indicates that I must specify a connection kit option that accompanies the DVP. Which appears contrary to when ordering the ST7MDT20-DVP?

Can anybody shed any light on this?

All the best,

Marty.
omar_12129
Associate
Aug 20, 2004 5:14 AM UTC
Posted on August 20, 2004 at 07:14

hello,

>So if I wanted to work with the TQFP64 (14x14) then in addition to ordering >the ST7MDT20-DVP3 I would have to order the ST7MDT20-T64/DVP also.

Yes

>So I will order an additional ST7MDT10-TEB/DVP. My first question is will I >get a default DIP16/SO16 kit with the TEB, or will I have to order this >seperately?

The ST7MDT10-TEB/DVP like the ST7MDT10-DVP3 include by default a DIP/SO package (DIP16/SO16 for ST7MDT10-DVP3)

>My other issue is that in the user guide for the ST7MDT10-DVP indicates >that I must specify a connection kit option that accompanies the DVP. >Which appears contrary to when ordering the ST7MDT20-DVP?

the connection option ordering is the same for ST7MDT20-DVP3 & ST7MDT10-DVP3. for example if you need DIP32/S032 you have to order ST7MD10-32/DVP.

Regards
md1
md1Author
Associate III
Aug 27, 2004 5:23 AM UTC
Posted on August 27, 2004 at 07:23

Thanks Ronaldo.