Skip to main content
Associate III
September 4, 2023
Question

Design help with load dump protection TVS

Need help with identifying the right TVS diode for load dump protection of our device. The test standard is MIL-STD-1275E which has 28V nominal working voltage with Ri = 0.5 ohm. The surge has a pulse duration of 50ms, Us = 100V, 5 number of pulses with a duration of 5 seconds in between two consecutive dumps.

I am not able to follow how Internal resistance of the source (Ri) and Diode ratings can be related. How can I get to a conclusion, if I have a requirement for 0.5 ohm? Datasheet has no mention about Ri resistance or any graphs that tells about the trend of Ri vs Us. Should diode be connected in series / parallel? Any SMD TVS diodes that can help withstand this surge? 

This topic has been closed for replies.