Skip to main content
ongth60
Associate III
May 11, 2005 6:29 AM UTC
Question

debugging tools

Posted on May 11, 2005 at 08:29

debugging tools

This topic has been closed for replies.

4 replies

ongth60
ongth60Author
Associate III
May 3, 2005 5:30 AM UTC
Posted on May 03, 2005 at 07:30

Hi all,

I would like to ask if the debugger has the ability to record the steps that have been run in the program to trace back the statements that have been executed? Pls advice.

Rgds,

TH Ong

ongth60
ongth60Author
Associate III
May 3, 2005 10:09 PM UTC
Posted on May 04, 2005 at 00:09

Hi,

Thanks for the info. Well,its going to be tough searching for a bug without this functionality.

Rgrds,

TH Ong

ongth60
ongth60Author
Associate III
May 4, 2005 12:33 AM UTC
Posted on May 04, 2005 at 02:33

Hi again,

Does Realview Trace provide the profiler functionality that I've wanted? Im using RealView Ice.

Rgrds,

TH Ong

weigelt
Associate
May 11, 2005 2:50 AM UTC
Posted on May 11, 2005 at 04:50

Hi,

using RealView ICE does not necessarily mean using RVDK, as the JTAG-Adapter shipped with RVDK is referred to as ''RealView ICE Micro Edition''. The RealView ICE is a tool that can be used with RVDS as well, connected to USB or Ethernet.

@ongth: I guess RealView Trace provides the needed functionality

regards,

Marcus