Skip to main content
ongth60
Associate III
May 5, 2005 10:14 AM UTC
Question

debugger startup error

Posted on May 05, 2005 at 12:14

debugger startup error

This topic has been closed for replies.

2 replies

ongth60
ongth60Author
Associate III
May 4, 2005 6:31 AM UTC
Posted on May 04, 2005 at 08:31

Hi,

I cant open my realview debugger v1.6.1. The startup warning states the following :

Cannot obtain license for RVD IDE Support (feature st_rvd_ide_D97137A7) with license version >=1.6:

Feature has expired

Feature: st_rvd_ide_D97137A7

Expired date: 30-mar-2006

License path: C:\Program files\ARM\Licenses\license.dat

FLEXIm Error: -10,32

For further information, refer to FLEXIm End User Manual,

available at ''www.macrovision.com''.

Specify the command line option '-cmd' to start RealView Debugger in non-graphical mode.

Pls advise.

ongth60
ongth60Author
Associate III
May 5, 2005 9:16 AM UTC
Posted on May 05, 2005 at 11:16

hi,

i've managed to solve the problem. It seems that I accidently adjusted the time clock of my taskbar to the date that exceeds the expiry date. When I adjusted it back to the real time, it wouldn't work. So, what I did was uninstall the whole IDE and install it back. It works fine now. Thanks anyway.