Skip to main content
benjaminpersbrant
Associate II
Feb 8, 2008 7:02 AM UTC
Question

debugg with st7 flash stick

Posted on February 08, 2008 at 08:02

debugg with st7 flash stick

This topic has been closed for replies.

5 replies

benjaminpersbrant
Associate II
Jan 30, 2008 6:53 AM UTC
Posted on January 30, 2008 at 07:53

Hello friends. I have a ST7 flash stick. I wondering is it possible to debugg a st7lite09 online with the ST7visual developer and the S7 flash stick?

Thanks.

Regards Ben

seb13_colin
Visitor II
Feb 4, 2008 5:19 AM UTC
Posted on February 04, 2008 at 06:19

Hello Ben,

I think it's not possible to perform In Circuit Debugging (ICD) on a st7lite09 part. I hope it's that you mean by ''debug online''. Indeed, there is not debug module on the chip. So you can only program it but not debug it.

Regards,

Seb

wolfgang2399
Associate III
Feb 4, 2008 5:58 AM UTC
Posted on February 04, 2008 at 06:58

Hi Ben,

it looks as if the STICK really is not suitable for online debugging.

I only found hints to applicable development tools in the manual at chapter 15.3 DEVELOPMENT TOOLS. Hope it will help you.

Regards,

WoRo

laurent239955_stm1
Associate
Feb 7, 2008 11:28 AM UTC
Posted on February 07, 2008 at 12:28

Hi,

STVD can debug through the ST7-STICK, this feature has been introduced since few monthes. As Seb13-colin told, the device need to have a debug module to support debugging whatever is the tool.

Best regards

Laurent

benjaminpersbrant
Associate II
Feb 8, 2008 7:02 AM UTC
Posted on February 08, 2008 at 08:02

Thanks for the reply.

Ben