Skip to main content
thibaut2
Associate III
Aug 30, 2012 10:11 AM UTC
Question

Debug/programming another chip with STLINK from STM8disco

Posted on August 30, 2012 at 12:11

Hi,

After developping and testing with stm8s-discovery connected to various evalboards, i just received my prototype.

As written in STM8SVLDISCOVERY's usermanual, i unsoldered the two 0 Ohms of swim connector from the STLINK (i don't want to break the discovery board yet).

Now, i disconnected everything on my board (thru jumpers), except external power-supply to the micro, and i connected SWIM port and GND.

The Chip i use is the STM8S105S4, and i already changed the device target.

Using STVD/Cosmic, i try to enter debug mode and i receive this message :

 

Starting debug session...

 

 -> Emulator reset (usb://usb)...

 

  ** Connection error (usb://usb): swim error [30006]: comm init error: chip does not answer

 

 

 -> Failed to connect target.

Seeing SWIM_reset pin, i also connected it (althrough SWIM = SingleWire) and i get same message :\

What did i miss ?
    This topic has been closed for replies.

    1 reply

    thibaut2
    thibaut2Author
    Associate III
    Aug 30, 2012 12:26 PM UTC
    Posted on August 30, 2012 at 14:26

    Well... I went for lunch, and after the break, everythin worked fine....

    I guess the computer was hungry too ^^