Skip to main content
jm2
Associate
Nov 25, 2003 5:33 PM UTC
Question

DEBUG Interface

Posted on November 25, 2003 at 18:33

DEBUG Interface

This topic has been closed for replies.

2 replies

jm2
jm2Author
Associate
May 17, 2011 9:57 AM UTC
Posted on May 17, 2011 at 11:57

Hi!

I'm designing a PCB with a µPSD3212 - but want to be able to put a µPSD3333 as an option.

A FLASH-Link Port for the µPSD is designed on the PCB. In addition to the µPSD3212 the µPSD3333 has a ''DEBUG''-pin.

What to do with this pin to be sure, that I can use the debugging-features? What external hardware do I have to use for debugging? I have the 3200 developement-board and the FLASH-Link-Interface for the printer-port. May I use this for a µPSD3333 as well? Will I be able to archive debugging-features with this?

Is there already a App-Note for the µPSD3333, that sums up the debugging-features?

Thanks very much![addsig]
joseph2399
Associate II
May 17, 2011 9:57 AM UTC
Posted on May 17, 2011 at 11:57

Please see the attached, AN1724 , Conversion Guide uPSD3200 to uPSD3300. Also attached, Application note AN1763, has a section on KEIL'S uLink USB-JTAG Debugger used on uPSD33xx.