Skip to main content
shinnlin
Associate III
Oct 28, 2004 7:30 AM UTC
Question

data bit rate on GPIO

Posted on October 28, 2004 at 09:30

data bit rate on GPIO

This topic has been closed for replies.

2 replies

shinnlin
shinnlinAuthor
Associate III
Apr 30, 2004 3:28 AM UTC
Posted on April 30, 2004 at 05:28

If I would like to use one GPIO pin as clock source of a pheripheral, that is send 0/1/0/1 sequence on that GPIO pin, anyone know the output data bit rate of it ?

( clock rate = 1/2 * data bit rate )

hacl
Visitor II
Oct 28, 2004 4:55 AM UTC
Posted on October 28, 2004 at 06:55

Dear forum,

I have some problems with the GPIO's too. I wrote a program only toggeling one GPIO-Pin. The MCLK works with 48 MHz and PCLK1, PCLK2 works with 24 MHz.

The toggel-frequency of the Out-Pin is only 146 kHz !!

I can't believe that this will be the maximum frequency of a GPIO. What can I do ?