Skip to main content
Amal Babu
Associate III
Dec 18, 2018 7:03 AM UTC
Question

Couldn't find the alternative function table specified for controller.

i am using STM8L101F1.I happen to go through the datasheet and i found that the pin of the IC can be multiplexed.But i couldn't find any registers specified with the alternate functions for the pins of the controller.

the following pins have the spi functions:

PB7:MISO

PB6:MOSI

PB5:SCK

PB4:SPI_NSS

how should i go about configuring these pins for spi function.

    This topic has been closed for replies.

    10 replies

    After Forever
    Senior III
    Dec 18, 2018 8:33 AM UTC

    In ST world, this kind of things are found not in the datasheet but in the reference manual - https://www.st.com/resource/en/reference_manual/CD00184503.pdf

    10.7.1 Alternate function input

    10.8.1 Alternate function output

    19.3.2 Configuring the SPI in slave mode

    19.3.3 Configuring the SPI master mode

    Amal Babu
    Amal BabuAuthor
    Associate III
    Dec 18, 2018 12:16 PM UTC

    PB_DDR = 0x04; 

    PB_ODR = 0x04;

    when i configure direction register Px_DDR only i'm not facing any issues, but when i configure Px_ODR the error shown below appears. I am using ST visual develop and compiler COSMIC.Is this issue due to lack of any header files. I have just added 2 header files .

    #include <iostm8.h>

    #include <stdio.h>

    #error cpstm8 main.c:22(1+6) PB_ODR undefined

    main.c:

     The command: "cxstm8 +debug -pxp -no -l +mods0 -pp -i"C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8" -clDebug\ -coDebug\ main.c " has failed, the returned value is: 1

    exit code=1.

    AvaTar
    Senior III
    Dec 18, 2018 8:58 AM UTC

    The actual pin-out and alternate function table for STM32's is located in the datasheet, not the reference manual.

    Other vendors put all in one document, not mentioning different naming preferences (datasheet, reference manual, hardware manual, etc. ).

    After Forever
    Senior III
    Dec 18, 2018 9:10 AM UTC

    True, but I was referring to this part (below) of the question, not the tables:

    > i couldn't find any registers specified with the alternate functions for the pins of the controller.

    Aren't the peripherals' registers descriptions in the RMs?

    BTW, not that it matters, but this is about STM8, not STM32.

    AvaTar
    Senior III
    Dec 18, 2018 12:36 PM UTC

    > BTW, not that it matters, but this is about STM8, not STM32.

    This mediocre forum software uses to hide large parts of a post - like in this case.

    But a speaking title for a thread (including the MCU it is about) is really helpful.

    Amal Babu
    Amal BabuAuthor
    Associate III
    Dec 18, 2018 11:44 AM UTC

    i configured spi mosi pin in pushpull mode as suggested by RM.

    PB_DDR |= 0x80;        

    PB_CR1 |= 0x80;

    BUT

    am getting the error shown below:

    #error cpstm8 main.c:24(1+6) PB_CR2 undefined

    #error cpstm8 main.c:23(1+6) PB_CR1 undefined

    main.c:

     The command: "cxstm8 +debug -pxp -no -l +mods0 -pp -i"C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8" -clDebug\ -coDebug\ main.c " has failed, the returned value is: 1

    exit code=1.

    why is that so?

    After Forever
    Senior III
    Dec 18, 2018 12:11 PM UTC

    Are you using the peripheral library? Maybe it already has the features you need for setting the alternate functions (I don't use it so I don't know).

    If not, then try to use GPIOB->DDR, GPIOB->CR1 and GPIOB->CR2 instead of PB_DDR, PB_CR1 and PB_CR2.

    Amal Babu
    Amal BabuAuthor
    Associate III
    Dec 18, 2018 12:20 PM UTC

    i have include <stm8l.h> but got an error

    #error cpstm8 main.c:4 can't open stml.h

    main.c:

     The command: "cxstm8 +debug -pxp -no -l +mods0 -pp -i"C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8" -clDebug\ -coDebug\ main.c " has failed, the returned value is: 1

    exit code=1.

    AvaTar
    Senior III
    Dec 19, 2018 7:38 AM UTC

    > #error cpstm8 main.c:4 can't open stml.h

    Your project is probably not properly setup, i.e. some system include paths are missing.

    > -l -i"C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8

    These are the include paths I can identify. Try locating stml.h in your file system, and add the path to the includes.

    Amal Babu
    Amal BabuAuthor
    Associate III
    Dec 19, 2018 8:24 AM UTC

    hai,

    thanks for the support, i could clear the issue by downloading different header files and including them in my code