Skip to main content
jrichards
Visitor II
Jul 3, 2011 9:15 PM UTC
Question

Cosmic CXSTM8 Comiler Error - Invalid Constant Expression

Posted on July 03, 2011 at 23:15

I'm porting some code designed to run on a Nordic nRF8200 to an STM8L152C6. The code was orginally compiled using Keil C5. I am using the Cosmic CXSTM8 compiler.

I am getting a compiler error 'Invalid Constant Expression' in the CASE: line of a switch statement that I cannot understand.

code snippet is included below.

switch (pipe_num)

  {

    case PIPE_LINK_LOSS_ALERT_ALERT_LEVEL_RX:

      alert_handle_on_link_loss = (alert_level_t)buffer[0];

      break;

     default:

       break;

  }

pipe_num is a locally defined uint8_t, and

 #define PIPE_LINK_LOSS_ALERT_ALERT_LEVEL_RX  6 is declared in an included header file.

I cannot understand what the compiler is taking exception to in this case. If anyone could help I'd really appreciate it.

    This topic has been closed for replies.

    1 reply

    Andrew Neil
    Super User
    Jul 4, 2011 6:58 AM UTC
    Posted on July 04, 2011 at 08:58

    ''I am getting a compiler error 'Invalid Constant Expression' in the CASE: line of a switch statement that I cannot understand''

    First, are there any other errors or warnings before this? If so, fix them

    first

    !

    You mean this line:

    case PIPE_LINK_LOSS_ALERT_ALERT_LEVEL_RX: 

    The only constant expression there is PIPE_LINK_LOSS_ALERT_ALERT_LEVEL_RX - so re-check that definition.

    Are you sure it isn't, for example, affected by some #if conditional compilation options that you've not (properly) set-up in your project...?

    Howver,

     alert_handle_on_link_loss = (alert_level_t)buffer[0];

    is also a constant expression - are you sure it's not complaining about that?

    ''I cannot understand what the compiler is taking exception to in this case''

    Have you tried looking at the preprocessor output?

    See: 

    http://www.8052.com/forum/read/29152

      It's not 8052-specific - and do make sure that you haven't made the very mistake mentioned there!

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.