Skip to main content
Aaron Derbyshire
Associate III
Jun 14, 2017 9:58 AM UTC
Solved

COSMIC Compiler structure initialisation

Posted on June 14, 2017 at 11:58

Currently I have an issue when trying to allocate a structure to RAM.

The issue I have is that my structure occupies a total of 373 bytes but the compiler/linker is insistent on trying to locate this structure in the zero page (first 256 bytes). To enable compilation I have reduced the size of the structure to allow for viewing of the map file to see where the compiler is allocating this data.

I have attempted to use the pragma directives to allocate this structure to the @near range, which would allow anywhere within the RAM space. This again gave me a section overflow of the zero page!

To go one step further I have defined my own section within the RAM space with the required size memory allocation. I have positioned this directly after the zero page and prior to the .data section. Using absolute addressing and the pragma directives I am still experiencing the same issues, or, now I have an error as the symbol has been defined for the zero page. I have e-mailed Cosmic but they don't seem to care for offering support.

Has anyone got any advice?

UPDATE: Just to add some further information.

- RAM size = 1024 bytes.

- Zero Page = 256 bytes.

- Max stack size 513 bytes (my thoughts are that this will be given the optimal size by the compiler/linker depending in the .data and .bss usage).

- Default linker file is being used, with the exception of the test section described above.

#ram #stm8 #cosmic #cosmic-stm8-cosmic-lkf
This topic has been closed for replies.
luca239955_stm1_st
Associate
Jun 14, 2017 4:26 PM UTC
Posted on June 14, 2017 at 18:26

Hello,

in order to put your structure (or any other variable) in the @near address space (out of page zero), you either have to specify the @near attribute for you structure or to use a memory model where this attribute is the default (+modsl0 is the usual choice for this).

If neither of these solutions seem to work please post your code here and I'll see what is wrong with it (I will also check with my colleagues if they have received your email on the support address).

Regards,

Luca

7 replies

luca239955_stm1_st
Associate
Jun 14, 2017 4:26 PM UTC
Posted on June 14, 2017 at 18:26

Hello,

in order to put your structure (or any other variable) in the @near address space (out of page zero), you either have to specify the @near attribute for you structure or to use a memory model where this attribute is the default (+modsl0 is the usual choice for this).

If neither of these solutions seem to work please post your code here and I'll see what is wrong with it (I will also check with my colleagues if they have received your email on the support address).

Regards,

Luca

Aaron Derbyshire
Associate III
Jun 15, 2017 9:48 AM UTC
Posted on June 15, 2017 at 09:48

Hi Luca,

Thanks for your response! A member of the Cosmic support team has now been in contact with me.

I have tried to use the space modifier, however, I am returned with a space attribute conflict error. Similarly this happens when using the pragma directives also. I will look at modifying the default memory model.

Thanks again,

Aaron

Aaron Derbyshire
Associate III
Jun 15, 2017 9:56 AM UTC
Posted on June 15, 2017 at 09:56

I have modified the default configuration file to use the stack long memory model and that has compiled first time and allocated my structure in the .data section as desired!

Thank you very much for your help!

Aaron