Skip to main content
krzysztof239955_st
Associate II
Nov 13, 2009 11:00 AM UTC
Question

Cosmic compiler - section boundary crossing

Posted on November 13, 2009 at 12:00

Cosmic compiler - section boundary crossing

    This topic has been closed for replies.

    5 replies

    krzysztof239955_st
    Associate II
    May 17, 2011 1:05 PM UTC
    Posted on May 17, 2011 at 15:05

    Hi,

    I use Cosmic compiler with STVD.

    The error receive after linking:

    #error clnk Debug\waga tw.lkf:34 Debug\beep.o: section boundary crossing (.text:018d) c_uitolx

    #error clnk Debug\waga tw.lkf:37 Debug\funkc.o: section boundary crossing (.text:0003) c_uitolx.

    How can one remove this error?

    Best regards.

    Kris.

    luca239955_st
    Associate II
    May 17, 2011 1:05 PM UTC
    Posted on May 17, 2011 at 15:05

    Hi,

    can you please send me, on my personal email (luca.ubiali@cosmic.fr)

    - the files interrupt_vector.c /.o /.ls

    - the compiler version you are using

    - the file crtsi.sm8

    I have to make some checks before I give you an answer.

    Regards,

    Luca

    krzysztof239955_st
    Associate II
    May 17, 2011 1:05 PM UTC
    Posted on May 17, 2011 at 15:05

    Hi Luca.

    I change memory model and libraries for code larger than 64K.

    The error receive after linking:

    #error clnk Debug\waga tw.lkf:1 prefixed symbol f__stext in conflict (C:\Program Files\COSMIC\CXSTM8\Lib\crtsi.sm8 Debug\stm8_interrupt_vector.o)

    #error clnk Debug\waga tw.lkf:1 symbol __stext not defined (Debug\stm8_interrupt_vector.o )

    Best regards.

    Kris

    luca239955_st
    Associate II
    May 17, 2011 1:05 PM UTC
    Posted on May 17, 2011 at 15:05

    Hello,

    looks like you are exceeding the 64k limit (for stm8, this actually means exceeding address 0xFFFF, which means 32k of code, since the flash starts at 0x8000), bot you are still using a memory model / libraries for smaller applications (you now need to use mod/lib that do not end with 0)

    Regards,

    Luca (Cosmic)

    luca239955_st
    Associate II
    May 17, 2011 1:05 PM UTC
    Posted on May 17, 2011 at 15:05

    just to close this thread, the problem was due to a wrong way to declare the interrupt vectors: the way used was ok for < 64k, but did not work for bigger applications.

    Cosmic recommends to declare the interrupt vectors in the following way, that works for all memory models / application sizes:

    /* INTERRUPT VECTORS TABLE FOR STM8

    * Copyright (c) 2007 by COSMIC Software

    */

    #define NULL 0

    extern void _stext(); /* startup routine */

    extern void recept(); /* character receive handler */

    #pragma section const {vector}

    void (* const @vector _vectab[32])() = {

    _stext, /* RESET */

    NULL, /* TRAP */

    NULL, /* TLI */

    NULL, /* AWU */

    NULL, /* CLK */

    NULL, /* EXTI PORTA */

    NULL, /* EXTI PORTB */

    NULL, /* EXTI PORTC */

    NULL, /* EXTI PORTD */

    NULL, /* EXTI PORTE */

    NULL, /* CAN RX */

    NULL, /* CAN TX */

    NULL, /* SPI */

    NULL, /* TIMER 1 OVF */

    NULL, /* TIMER 1 CAP */

    NULL, /* TIMER 2 OVF */

    NULL, /* TIMER 2 CAP */

    NULL, /* TIMER 3 OVF */

    NULL, /* TIMER 3 CAP */

    NULL, /* USART TX */

    recept, /* USART RX */

    NULL, /* I2C */

    NULL, /* LINUART TX */

    NULL, /* LINUART RX */

    NULL, /* ADC */

    NULL, /* TIMER 4 OVF */

    NULL, /* EEPROM ECC */

    NULL, /* Reserved */

    NULL, /* Reserved */

    NULL, /* Reserved */

    NULL, /* Reserved */

    NULL, /* Reserved */

    };

    the linker file should contain the lines

    +seg .vector -b 0x8000 -m 0x80 -k # vectors start address

    vector.o # interrupt vectors

    (sorry if it's not too clear, the CODE tag does not seem to work properly on the forum..)