Skip to main content
jarek
Visitor II
Feb 14, 2011 8:10 AM UTC
Question

Cosmic and @eeprom

Posted on February 14, 2011 at 09:10

Cosmic and @eeprom

    This topic has been closed for replies.

    2 replies

    luca239955_stm1_st
    Associate
    May 17, 2011 1:11 PM UTC
    Posted on May 17, 2011 at 15:11

    Hi,

    from the user manual, page 51:

    ****

    The library routines are also using a few external symbols to locate the command registers in the I/O register space. When a standard header file provided with the

    compiler is included in at least one source file of the application, these

    symbols are automatically found. Otherwise, it is necessary to provide

    these symbols either by extra C declarations...

    ****

    Regards,

    Luca

    saranyim
    Associate II
    May 17, 2011 1:11 PM UTC
    Posted on May 17, 2011 at 15:11

    I'm using EEPROM in different way. I'm not sure that just declare variable in eeprom arae.

    here is my source code 

    void EEPROM_WRITE(u16 addr,u8 data){

    FLASH_Unlock(FLASH_MEMTYPE_DATA);

    addr = 0x4000 + addr;

    FLASH_ProgramByte(addr, data);

    FLASH_Lock(FLASH_MEMTYPE_DATA);

    }

    u8 EEPROM_Read(u16 addr){

    u8 returndata;

    FLASH_Unlock(FLASH_MEMTYPE_DATA);

    addr = 0x4000 + addr;

    returndata =  FLASH_ReadByte(addr);

    FLASH_Lock(FLASH_MEMTYPE_DATA);

    return returndata;

    }

    to use EEPROM in my way you need to include STM8S_FLASH.C and .H from ST Standard Library into your project

    Saran