Skip to main content
firoz3321
Associate
October 19, 2020
Solved

Controller recommendation for migrating from to now available controller

Hi We have a product in market which uses UPSD3234  controller.

Can someone please suggest a controller that can be used to replace this with minimal code changes that supports

  1. USB2.0 or above and
  2. has more than one UART
  3. Ethernet (optional)

Thank you.

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    October 19, 2020

    This will be almost impossible due to your requirement of "minimal code changes": the UPSD3234 was a 8032 based MCU, which is completely different from the microcontrollers currently provided by STMicroelectronics (STM8/STM32/etc).

    Of course you can start a new project that has the same behavior as the one with the UPSD3234, but an STM8 does not offer any USB functionality. You should therefore select a device from the STM32 family, e.g. the STM32F407.

    Good luck!

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    2 replies

    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    October 19, 2020

    This will be almost impossible due to your requirement of "minimal code changes": the UPSD3234 was a 8032 based MCU, which is completely different from the microcontrollers currently provided by STMicroelectronics (STM8/STM32/etc).

    Of course you can start a new project that has the same behavior as the one with the UPSD3234, but an STM8 does not offer any USB functionality. You should therefore select a device from the STM32 family, e.g. the STM32F407.

    Good luck!

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    firoz3321
    firoz3321Author
    Associate
    October 19, 2020

    Thank you. We will look into the STM32 series.