Connection between EVLSPIN32G0B2 and ST-LINK/V2
Hi guys,
This is my first topic and I hope this is the right section.
I’m trying to connect the EVLSPIN32G0B2 evaluation board to the ST.LINK/V2 program tool connected to PC via USB.
When I click on Connect on the STM32CubeProgrammer I get the error “ST-LINK error (DEV_CONNECT_ERR)”.
Of course, when I do this I have the evaluation board connected to another usb port in order to supply the micro.
Why doesn’t it works? I can’t find my error.
I have another question: which is the program to be loaded on the EVLSPIN32G0B2 to make it working with Motor Pilor and be able to configure my brushless motor ?
Thank you
Stefano
EDIT:
I didn’t mentioned that the ST-LINK is connected to the EVLSPIN32G0B2 via a cable coded ARM-JTAB-20-10 bought on Mouser Electronic’s site and it is connected to the RESERVED connector on the EVLSPIN32G0B2 board.