Skip to main content
vivek2dy
Visitor II
Sep 20, 2016 9:54 AM UTC
Question

Configuring channel 1 of Timer1 for PWM signal (STM8S controller)

Posted on September 20, 2016 at 11:54

Hi,

We are working on STM8S003f3 microcontroller. We have successfully configured Channel 3 of the microcontroller.

When Tim1- Channel1 is configured in similar way, it does not produce PWM ouptput on the pin.

We have also enabled Option byte -AFR0 for selecting alternative function in 'ST Visual develop tool'.

Please refer code below for reference,

&sharpinclude ''STM8S003k3.h''

&sharpifndef BIT 

&sharpdefine BIT(n) (1 << (n)) 

&sharpendif

void PWM_OC1_25_OC2_50_OC3_75(void) 

{ 

TIM1_CR1&=~BIT(0); // Close TIM1

TIM1_PSCRH = 0; 

TIM1_PSCRL = 0; // undivided

TIM1_ARRH = 0; 

TIM1_ARRL = 99; 

TIM1_CCR1H = 0; 

TIM1_CCR1L = 25; // 25% duty cycle (25 / (99 + 1)) 

TIM1_CCMR1 = 0x60; // PWM mode 1 

TIM1_CCER1|=BIT(0); // Enable OC1 

TIM1_CCR3H = 0; 

TIM1_CCR3L = 75; // duty cycle of 75% (75 / (99 + 1)) 

TIM1_CCMR3 = 0x60; // PWM mode 1 

TIM1_CCER2|=BIT(0); // enable OC3 

TIM1_CR1|=BIT(0); // Enable TIM1 

TIM1_BKR|=BIT(7); // ban brakes 

}

main()

{

    PWM_OC1_25_OC2_50_OC3_75();    

    while (1);

} 

Any help would be greatly appreciated.

Thanks and Kind Regards,

Vivek 

#stm8s-tim1_ch1
    This topic has been closed for replies.

    3 replies

    Marcio Segura
    Visitor II
    Jun 8, 2017 4:56 PM UTC
    Posted on June 08, 2017 at 18:56

    Did you get this issue? I am also struggling to solve it, I could make Channel 3 and 4 work but not 1 and 2.

    Tom Schrauf
    Associate II
    Oct 1, 2017 9:41 PM UTC
    Posted on October 01, 2017 at 23:41

    Hello !

    Well June is quite a while ago ....

    I'm also using the 20 pin version and it did not work at first try either - although the setting of the option bit seemed correct it was not set properly by the programmer. So i think that is what likely happened to you too.

    This option flags reside in flash at address 0x4803 and 0x4804 and values should be 0x01 and 0xFE (the complement). In debugger open a memory window and inspect content:

    004800  00 00 FF 01 FE 00 FF 00 ........  <- should look like this

    004800  00 00 FF 00 FF 00 FF 00 ........  <- this is default with AFR1 reset (SPI instead of TIMER channels)

    You cannot change these at runtime (easily) but have to set the options bits correctly in the IDE.

    Tom

    Philip Haasnoot
    Associate
    Dec 6, 2017 8:54 PM UTC
    Posted on December 06, 2017 at 20:54

    Tom thank you for the reply, I am also struggling to get TIM1 to work. What is the best way to reconfigure the programmer to update 0x4803 and 0x4804.