Skip to main content
alain239955_st
Associate
Dec 17, 2009 7:52 AM UTC
Question

Configure Boot flash using Usb Jlink or Ulink

Posted on December 17, 2009 at 08:52

Configure Boot flash using Usb Jlink or Ulink

This topic has been closed for replies.

17 replies

alain239955_st
Associate
May 17, 2011 7:31 AM UTC
Posted on May 17, 2011 at 09:31

YES :D

It's working

Thank you for the help

[ This message was edited by: acorchia on 31-08-2006 15:47 ]

wwin2000
Associate
May 17, 2011 7:31 AM UTC
Posted on May 17, 2011 at 09:31

hi,STARM and acorchia: ''The CPU crashes because the FMI_Config function writes in the configuration registers of the flash which are located in Bank1.'' As i know the configuration registers of the flash is in 0x54000000~0x58000000 and bank1 flash address can be remap to 0x00000000~0x03ffffff. why you say that?

Regards

roger_lynx
Associate II
May 17, 2011 7:31 AM UTC
Posted on May 17, 2011 at 09:31

 

On 06-09-2006 at 09:44, acorchia wrote:

 

Hello,

 

 

I Did buy the RLINK USB limited version.

 

I Use it with CAPS to update confuguration data. it is working without any problems

 

Thanks for your input, I got Rlink (from Digikey), and brought my 911 (no, not from Porsche) board up.

It works, I do apologize for my previous bitching about ST tools.

Now, if I could burn the config. bits with my JLink.....?

roger_lynx
Associate II
May 17, 2011 7:31 AM UTC
Posted on May 17, 2011 at 09:31

 

I Use it with CAPS to update confuguration data.

 

it is working without any problems

 

Thanks for your feedback.

kurt2399
Visitor II
May 17, 2011 7:31 AM UTC
Posted on May 17, 2011 at 09:31

The HiTOP Debugger and IDE which is included in the Hitex STR9 starterkit supports the FLASH configuration as well as the LVD treshold settings. These can be configured easy with the seetings dialog.

Best regards

Kurt

ug_it
Visitor II
May 17, 2011 7:31 AM UTC
Posted on May 17, 2011 at 09:31

Hi all,

look here to find KEIL's solution for selecting STR91x Flash banks using the ULINK adapter:

http://www.keil.com/support/docs/3347.htm

I'm using this method to select the boot bank1 for my IAP bootloader successfully.

Hope this helps.

Ullrich

rmichon
Visitor II
May 17, 2011 7:31 AM UTC
Posted on May 17, 2011 at 09:31

Hi all,

to set the bank 1 as the boot bank on the st9 using jlink, you can use the Segger j-link tools.

you can find them here:

SEGGER

open the folder with command line and call jlinkstr91x.exe.

it should connect through jlink. you then have to type 'setb 1' and you're done. the boot bank will be the bank 1.

hope it helps!

cheers,

Bib'