Skip to main content
jendao2000
Associate
Jul 4, 2004 8:13 AM UTC
Question

compiler C to OBJ & HEX (for DK3200)

Posted on July 04, 2004 at 10:13

compiler C to OBJ & HEX (for DK3200)

This topic has been closed for replies.

5 replies

bbbodekar
Associate III
May 17, 2011 10:02 AM UTC
Posted on May 17, 2011 at 12:02

Hi

I guess you can ask the dealer from where you got the DK3200 to give you an evaluation copy of the C compiler, which would give you both the obj and hex files. You can use Keil C compiler for the same. I dont rember if you get is along with the DK3200 kit. Check it out

Wish you good luck and prosperity in your business!

jendao2000
Associate
May 17, 2011 10:02 AM UTC
Posted on May 17, 2011 at 12:02

Hello !

i am a newbie in this bussiness and I need your immediate help .

Where can I get a compiler from C to OBJ and HEX?

Thanks for your attention .

jeniok

sjo
Associate III
May 17, 2011 10:02 AM UTC
Posted on May 17, 2011 at 12:02

There are numerous compilers available for the upsd, any which support 8032 core.

Have a look at www.keil.com, www.raisonance.com, www.tasking.com etc.

If you want to go the free route have a look at sdcc

http://sdcc.sourceforge.net

Regards

sjo
jendao2000
Associate
May 17, 2011 10:02 AM UTC
Posted on May 17, 2011 at 12:02

Can you send me the exact link where I can download the compliler?

There are many compilers and I don't find where to download the one I need, I don't know which one I need to compile from C to OBJ and HEX.
bbbodekar
Associate III
May 17, 2011 10:02 AM UTC
Posted on May 17, 2011 at 12:02

Yes sjo is right.

For DK3200 using UPSD3200, you need to have Keil C compiler. With this, you can compile may devices, e.g Philips 5051 core family , Philips 8032 famliy processors or Cygnal processors etc. So you are not restricted with only 1 type of devices. You get a demo CD from them which has got demo programs and tutorials for using the Keil compiler.

Have fun !