Skip to main content
mtignor
Associate
Apr 16, 2006 6:40 PM UTC
Question

Choices of C Compilers for ST7F part?

Posted on April 16, 2006 at 20:40

Choices of C Compilers for ST7F part?

This topic has been closed for replies.

10 replies

mtignor
mtignorAuthor
Associate
Feb 6, 2006 4:18 PM UTC
Posted on February 06, 2006 at 17:18

I am looking at the alternatives for ST7F tools for C compiler and debug. I have a package from Cosmic. Are the any other choices? I see Metrowerks listed in web pages at Softecmicro. But I can't find much more info than this.

Are these the only two choices? - thanks, Mike

wolfgang2399
Associate III
Feb 7, 2006 5:09 AM UTC
Posted on February 07, 2006 at 06:09

Hi Mike,

I've never heard of any other C-Compiler for ST7 than Cosmic and Metrowerks.

I use the Metrowerks and the STVD7 (visual develop) from STMicro and I am comfortable with both of them.

You can download the STVD7 from the

http://mcu.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=15

and use it for free. It is a quite practical tool.

You may use the STVD7 with the Cosmic as well.

Regards

WoRo

Viktor POHORELY
ST Employee
Feb 7, 2006 7:32 AM UTC
Posted on February 07, 2006 at 08:32

I will strongly recommend to use Cosmic in combination with STVD7 toolchain.

sylv1laurent
Visitor II
Feb 8, 2006 4:18 PM UTC
Posted on February 08, 2006 at 17:18

Hi Mike,

I have developed an IP stack on ST7F321 with C-Cosmic and several routine in asm with an EMU3.

This emulator is very good to develop and debug complex application.

I have had lot of problems with cosmic C to integrate C and ASM, especialy for routine parameter and variable declaration.

Regards

Sly

luter
Associate III
Feb 9, 2006 2:39 AM UTC
Posted on February 09, 2006 at 03:39

Hi.

I use Cosmic since 1 year and I am satisfied. I did not have any big problems due to compiler.

luca239955_st
Associate II
Feb 9, 2006 5:59 AM UTC
Posted on February 09, 2006 at 06:59

Quote:

....

I have had lot of problems with cosmic C to integrate C and ASM, especialy for routine parameter and variable declaration.

What problems?

Just curious.

Regards,

Luca (Cosmic)

wolfgang2399
Associate III
Feb 9, 2006 6:04 AM UTC
Posted on February 09, 2006 at 07:04

Hi Setler,

I've never had any problems with Cosmic using the STVD7 - but I don't have any after I've changed to the Metrowerks C-compiler.

So why do you ''strongly recommend'' to use the Cosmic compiler???

Regards

WoRo

xpcommon
Visitor II
Feb 9, 2006 3:29 PM UTC
Posted on February 09, 2006 at 16:29

Hi new here, i would rather prefer STVD7

sisto
Associate II
Apr 15, 2006 12:09 PM UTC
Posted on April 15, 2006 at 14:09

I will strongly recommend to use Cosmic in combination with STVD7 toolchain.

I vote at all !!

I use Cosmic ''C'' compiler from about 4 years without any problem... You can believe to me !

So You can just investigate if You are using it correctly.

The Cosmic support service is very efficient to help You about any problem You have.

Sixtus

info45
Associate
Apr 16, 2006 6:40 PM UTC
Posted on April 16, 2006 at 20:40

Hy,

I use MW and Cosmic also .

I recommend Cosmic because: Hiware was acquired by Metrowerks, and Metrowerks , now, is part of Freescale ( ex Motorola).

Then I thinks that Metrowerks don't will support new micro, function and support for ST enviroment...

By