Skip to main content
carnett1
Associate III
Dec 14, 2010 12:49 PM UTC
Question

CCO

Posted on December 14, 2010 at 13:49

has anybody ever used CCO, the configurable Clock Output?  I think I initialized it.  I enabled it.  Everything compiled but I never did anything that would set the frequency.  The output is a high.  Does anyone know of an example or what I should be doing?  I look thru the manuals and nothing seems to help me.  It seems like such a simpe function but it is difficult for me.

charles

    This topic has been closed for replies.

    2 replies

    spiovan9
    Associate III
    Dec 16, 2010 5:37 PM UTC
    Posted on December 16, 2010 at 18:37

     Â»  Â»  Â»  Â»  Â» 

    examples/TIM1/TIM1_Input_Capture/main.c

    00001

    /**

    00002

    ******************************************************************************

    00003

    * @file TIM1_Input_Capture\main.c

    00004

    * @brief This file contains the main function for TIM1 Input Capture example.

    00005

    * @author STMicroelectronics - MCD Application Team

    00006

    * @version V1.1.1

    00007

    * @date 06/05/2009

    00008

    ******************************************************************************

    00009

    *

    00010

    * THE PRESENT FIRMWARE WHICH IS FOR GUIDANCE ONLY AIMS AT PROVIDING CUSTOMERS

    00011

    * WITH CODING INFORMATION REGARDING THEIR PRODUCTS IN ORDER FOR THEM TO SAVE

    00012

    * TIME. AS A RESULT, STMICROELECTRONICS SHALL NOT BE HELD LIABLE FOR ANY

    00013

    * DIRECT, INDIRECT OR CONSEQUENTIAL DAMAGES WITH RESPECT TO ANY CLAIMS ARISING

    00014

    * FROM THE CONTENT OF SUCH FIRMWARE AND/OR THE USE MADE BY CUSTOMERS OF THE

    00015

    * CODING INFORMATION CONTAINED HEREIN IN CONNECTION WITH THEIR PRODUCTS.

    00016

    *

    00017

    * <h2><center>&copy; COPYRIGHT 2009 STMicroelectronics</center></h2>

    00018

    * @image html logo.bmp

    00019

    ******************************************************************************

    00020

    */

    00021 00022

    /* Includes ------------------------------------------------------------------*/

    00023

    #include ''''

    00024 00025

    /**

    00026

    * @addtogroup TIM1_Input_Capture

    00027

    * @{

    00028

    */

    00029 00030

    /* Private typedef -----------------------------------------------------------*/

    00031

    /* Private define ------------------------------------------------------------*/

    00032

    /* Private macro -------------------------------------------------------------*/

    00033

    /* Private variables ---------------------------------------------------------*/

    = 2000000; = 0; =0, =0; 00037

    /* Private function prototypes -----------------------------------------------*/

    00038

    /* Private functions ---------------------------------------------------------*/

    00039

    /* Public functions ----------------------------------------------------------*/

    00040 00041

    /**

    00042

    * @brief Example firmware main entry point.

    00043

    * @par Parameters:

    00044

    * None

    00045

    * @retval

    00046

    * None

    00047

    */

    void

    (

    void

    ) 00049 { 00050 00051 ( , , , , 0x0); 00052 00053

    /* Enable TIM1 */

    00054 (); 00055 00056

    /* Clear CC1 Flag*/

    00057 (); 00058 00059

    /* Connect LSI to COO pin*/

    00060 (, , ); 00061 (); 00062 (); 00063 00064 00065

    /* wait a capture on CC1 */

    00066

    while

    ((->SR1 & ) != ); 00067

    /* Get CCR1 value*/

    00068 = (); 00069 (); 00070 00071

    /* wait a capture on cc1 */

    00072

    while

    ((->SR1 & ) != ); 00073

    /* Get CCR1 value*/

    00074 = (); 00075 (); 00076 00077

    /* Compute LSI clock frequency */

    00078 = (8 * ) / ( - ); 00079 00080

    /* Insert a break point here */

    00081

    while

    (1); 00082 } 00083 00084 00085

    #ifdef USE_FULL_ASSERT

    00086 00087

    /**

    00088

    * @brief Reports the name of the source file and the source line number

    00089

    * where the assert_param error has occurred.

    00090

    * @param file: pointer to the source file name

    00091

    * @param line: assert_param error line source number

    00092

    * @retval

    00093

    * None

    00094

    */

    00095

    void

    assert_failed(* file, line) 00096 { 00097

    /* User can add his own implementation to report the file name and line number,

    00098

    ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */

    00099 00100

    /* Infinite loop */

    00101

    while

    (1) 00102 { 00103 } 00104 } 00105

    #endif

    00106 00107

    /**

    00108

    * @}

    00109

    */

    00110 00111

    /******************* (C) COPYRIGHT 2009 STMicroelectronics *****END OF FILE****/

    spiovan9
    Associate III
    Dec 16, 2010 5:41 PM UTC
    Posted on December 16, 2010 at 18:41