Skip to main content
tj2
Associate III
March 27, 2008
Question

Cannot exit StandbyMode on RTC alarm

  • March 27, 2008
  • 14 replies
  • 2178 views
Posted on March 27, 2008 at 06:41

Cannot exit StandbyMode on RTC alarm

This topic has been closed for replies.

14 replies

tj2
tj2Author
Associate III
October 24, 2005
Posted on October 24, 2005 at 07:21

Hi.

I cannot get our target board to wakeup from the RTC alarm. The code is working on the MB393B demoboard. So I think it's hardware related. But I cannot determine where the problem could be. I've verified the 32KHz clock and it is running...

ben2
Associate III
October 24, 2005
Posted on October 24, 2005 at 07:29

is you main oscillator running ? To exit from any mode apart from wfi and lpwfi the main oscillator must be running

tj2
tj2Author
Associate III
October 24, 2005
Posted on October 24, 2005 at 07:30

Yes, the main oscillator is running.

tj2
tj2Author
Associate III
October 24, 2005
Posted on October 24, 2005 at 10:58

On the MB393B board J3 is fitted.

On our board a 1µF ceramic capacitor is connected between V18BKP (pin 55) and VSSBKP. VSSBKP is connected to GND. And there is not an external power source is connected to the V18BKP pin.

tj2
tj2Author
Associate III
October 25, 2005
Posted on October 25, 2005 at 07:41

I've measured the voltage on the V18BPK pin and it was only 1.56V. Is this voltage too low for the RTC to operate?

tj2
tj2Author
Associate III
October 25, 2005
Posted on October 25, 2005 at 07:56

The voltage on the V18pin is 1.85V when not in standby, and drops to the 1.56V when entering standby mode.

tj2
tj2Author
Associate III
October 25, 2005
Posted on October 25, 2005 at 09:12

The Standby pin does not go high. There is a 100k pull-up connected to the pin.

When using the wake up pin the wake-up function correctly.

tj2
tj2Author
Associate III
October 25, 2005
Posted on October 25, 2005 at 09:19

I've just changed PCU_LPMEnter ( PCU_STANDBY ); to PCU_LPMEnter ( PCU_STOP );

And here the RTC wake up function correctly. So it is somehow related to the standby mode.....

tj2
tj2Author
Associate III
October 25, 2005
Posted on October 25, 2005 at 10:55

I made another test:

I thought maybe the 32KHz crystal didnt function during standby mode, so I made a program where the RTC_CounterValue() is send to the PC trough the UART. And the result is that the RTC _is_ running during standby. So I cannot understand why the alarm function wont work.

tj2
tj2Author
Associate III
October 25, 2005
Posted on October 25, 2005 at 11:58

The example is working on the MB393B demo board.

But not on our board. - The CPU never wakes up again and a reset or a logic high on the wake up pin is necessary.