Skip to main content
jade
Visitor II
Jul 13, 2011 5:43 AM UTC
Question

Cannot connect ST-Link

Posted on July 13, 2011 at 07:43

I am trying to program a hex file in STM8S103F2P6 using ST-Link via STVP

However, I get the error

> Programming  PROGRAM MEMORY area...

Error : Cannot communicate with the board.

Wrong board selection or check board power supply or check that a previous session is closed.

Error : < PROGRAM MEMORY programming failed.

Configuration:

Windows SP3, 

STLINK V1, 

Firmware: V1.J12.S3 JTAG+SWIM Debugger

Target: STM8S103F2P6

Is there another utility that can be used to program STM8S via ST-Link.

Thanks.

#stlink #stm8-swim-connect
This topic has been closed for replies.

2 replies

daveroffey9
Associate
Jul 14, 2011 8:39 PM UTC
Posted on July 14, 2011 at 22:39

That comes as no surprise to me. I have to do the same with STVD in win 7, and also edit the project file to fix the 'abslist' name in the postlink for building asm on two other pc's not win 7. Patch or no patch.

I know it doesn't help, but at least you know you are not alone in your quest for clean software.

newtonpro
Associate
Sep 6, 2011 8:15 AM UTC
Posted on September 06, 2011 at 10:15

I have 2 computers, a new one (called FIRST) and an old one (called SECOND).

On the NEW computer STDV is OK, but I have only the STDV program.

On the SECOND computer I have the old software for ST7 AND the STDV, but the STDV is displaying the message:'' Error : Cannot communicate with the board''. The ST7 software isn't ST trade and probably there are some conflicts between the drivers. I am going to format the SECOND and I will try to install only the STVD as first step.