Skip to main content
KMcGr.1
Visitor II
September 19, 2020
Question

Cannot compile code without stm8_interrupt_vector.c being brought into my project despite removing it from project.

I am trying to implement the "Delay" function from timing_delay.h / timing_delay.c that comes with STM8 example code. In order for the delay to work, you need to add the function "TimingDelay_decrement" to stm8l15x_it.c in order to decrement the timer (or it will go on forever).

You can only have one of the following files in a project without it breaking, either "stm8_interrupt_vector.c" or "stm8l15x_it.c". Everytime I build my code, stm8_interrupt_vector.c gets added to my project and breaks the build, despite the file not even existing at this point (removed any trace of it).

1) first and foremost, I really just want a delay function that works in my code.

2) second most I would not mind imeplementing the decrement function inside stm8_interrupt_vector.c, however I do not know how to do it.

3) lastly, I would like to figure out how to remove stm8_interrupt_vector.c from my project for good.

any of these three will do the trick I believe.

    This topic has been closed for replies.

    1 reply

    Visitor II
    April 17, 2025

    Hello Sir ,

     

    for delay Function in STM8S refer below Document

    https://boseji.com/posts/stm8-precise-cycle-delay/
    in this writer created a delay_cycles function and called it wherever he wants to implement delay.
    Note: pass bigger number than 1000 so that you will get more delay 

     For the  stm8_interrupt_vector.c  file follow below step in STVD IDE 
    1. Right Click on stm8_interrupt_vector.c   then go  to the Setting  then on top right side Click on "Exclude file from Build" and the rebuild your code .



    Thank You.