Skip to main content
cd_it
Visitor II
Mar 18, 2011 3:24 PM UTC
Question

Cannot communicate with STM8L-Discovery on W7-64

Posted on March 18, 2011 at 16:24

I have just purchased the STM8L-DISCOVERY, I have problems getting the device communication functioning on my primary PC. I have installed all the same apps... on a secondary PC, on this PC all is OK.

On my primary PC I get:

 ** Connection error (usb://usb): swim error [30004]: comm timeout

from the ST Visual Develop.

I have tried several solutions, without luck, and I suspect a OS issue.

The primary PC, is W7-64 bit, the secondary PC is W7-32bit.

Thanks

Casper Dietrich

#stm8l-discovery-64bit
    This topic has been closed for replies.

    3 replies

    infiniium
    Associate
    Apr 10, 2011 9:12 AM UTC
    Posted on April 10, 2011 at 11:12

    I am using STM8L Discovery on Win7 64bit.

    I have same error at first. But I found solution to solve.

    The error is occurred when I connect one to the USB HUB. But I connect it directly to the PC. Error is not shown.

    Please try.

    Stm32User
    Associate III
    Apr 13, 2011 2:31 PM UTC
    Posted on April 13, 2011 at 16:31

    Just an idea....

    Try running STVD in a compatibility mode.

    From START right click on stvd and click PROPERTIES.

    On COMPATIBILITY tab try one of the various options.

    stephane serre_O
    Visitor II
    Apr 13, 2011 3:01 PM UTC
    Posted on April 13, 2011 at 17:01

    Hi Casper,

    A new ST toolset pack version will be available by 1 or 2 weeks on

    http://www.st.com/

    .

    It will support W7 64bit and also fix the issues encountered when trying to get the STM8L-Discovery device communicting with PCs.

    Best Regards