Skip to main content
Associate III
February 15, 2024
Question

Cannot access >=3,3V at GPIOA - STM32F411

  • February 15, 2024
  • 46 replies
  • 16310 views

Dear Ladies and Gentlemen,

 

for you it is your daily business - for me as customer a contemporary challenge:

 

Something went wrong with my pin-configuration.

I measure ~1,7 V as GPIO-output of Port A instead of wished >=3.3 V.

My power supply is a USB.

Could you give a sample pin configuration for (3.3 V output) of Port A in discussion?

 

As additional comment:

Round about 5 V are present at the 5 V-Pin(s).

 

Thank you in advance.

TIMBO

 

This topic has been closed for replies.

46 replies

mƎALLEm
ST Technical Moderator
February 15, 2024

Hello,

Which board you are using? a custom board?

You need to provide schematics as well. 

".. instead of wished >=3.3 V." -> that depends on your VDD.  What is your VDD level?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Peter BENSCH
ST Technical Moderator
February 15, 2024

The TO talks about the Black Pill, probably this one.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
February 15, 2024

Reduce the load attached to the pin. Perhaps just remove and measure then.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
timbo2023Author
Associate III
February 15, 2024

It is a BlackPill (weact v. 3.0) -

 

To my purpose - I need the round about 5 V from 5 V-Pin at the outputs of PA0-PA3.

 

~ 3.3 V would be enough, but I measure ~1.7 V at the moment...

 

It seems to be a configuration thought...

mƎALLEm
ST Technical Moderator
February 15, 2024

BlackPill/BluePill are not boards of ST and unfortunately some of them have fake STM32 on them!

Meanwhile, even with a genuine STM32 you can't reach 5V. The maximum you can reach is 3.6V which is the maximum of VDD.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
timbo2023Author
Associate III
February 15, 2024

Ohhwee, that we must consider & check, of course.

 

On the 5 V pin were 4. ..V with USB given.

Is it possible to reach this voltage direct on another pin of port A?

But:

~3.6 V would be enough - VDD - of course - How looks the configuration of the pin0-3 of port A regarding it?

 

timbo2023Author
Associate III
February 15, 2024

Thank you, Mr. NEIL - ok, that i understood with support of your answer.

 

But back to VDD with its reachable value - I measure after a pin configuration ~1.7 V - how should be the configuration to reach the "full" 3.6 V on the pins of port A.

 

Could you give a sample?

 

 

mƎALLEm
ST Technical Moderator
February 15, 2024

Could you please share your GPIO config?

This is what you need to toggle PA2 pin for example:

 

 __HAL_RCC_GPIOA_CLK_ENABLE();

 GPIO_InitStruct.Pin = GPIO_PIN_2;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
 HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
 
 while (1)
 {
 HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_2);
 /* Insert delay 100 ms */
 HAL_Delay(100);
 }

 

With this code PA2 pin will be at VDD level (let's say @3.3V) during 100ms and 0V at the same duration ..

 

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
timbo2023Author
Associate III
February 15, 2024

Ok, thank you -

"bare metal" or some more fundamental input, please - we sit in GER not in USA or RUSSIA ...

 

But as qualified input:

You set the GPIOx_MODE-register to "general purpose output mode" - that we understand.

You set GPIOx_PUPDR to "No pull-up, pull-down" =^ "00"

You set GPIOx_OSPEEDR to "low speed" =^ "00"

 

I will try it.

 

But is the ODR-value the same like the BSRR-value in look to this case?

 

 

 

 

 

 

 

Tesla DeLorean
Guru
February 15, 2024

Perhaps graduate to bare-metal when you have other things mastered.

What are you attempting to drive with the pin? A Motor?

Does PA3 conflict with anything else on your board? What's connected? Diagram.

The current out of the pin is limited, If you're getting 1.7V the load is likely too high. Remove the load and measure the pin level then.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
timbo2023Author
Associate III
February 15, 2024

I measure to the board ...

 

something went wrong here ...

 

 

 

mƎALLEm
ST Technical Moderator
February 15, 2024

Again please share your code to conclude. This is not the right way to help you efficiently by doing ping pongs comments!

How did you configure the GPIO(s)? 

""bare metal" or some more fundamental input, please - we sit in GER not in USA or RUSSIA ..."

--> Start with HAL then move to direct access to the registers ..

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
timbo2023Author
Associate III
February 15, 2024

I got round about 3.3 V on PA1-3.

I got round about 1.7 V on PA0.

mƎALLEm
ST Technical Moderator
February 15, 2024

@timbo2023 wrote:

I got round about 3.3 V on PA1-3.

I got round about 1.7 V on PA0.


Check what is connected to PA0. Is there something connected to it?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
timbo2023Author
Associate III
February 15, 2024

Where I can reach the 3.6 V ?

mƎALLEm
ST Technical Moderator
February 15, 2024

@timbo2023 wrote:

Where I can reach the 3.6 V ?


As I said previously, the GPIO output high level depends on your VDD. If your VDD is at 3.3V, your pin can't go more than 3.3V!

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.