Skip to main content
hg-chen
Associate III
Jan 9, 2008 8:12 AM UTC
Question

Can USB_clk pin of STR9 used as GPIO even USB function enable?

Posted on January 09, 2008 at 09:12

Can USB_clk pin of STR9 used as GPIO even USB function enable?

This topic has been closed for replies.

2 replies

hg-chen
hg-chenAuthor
Associate III
May 17, 2011 7:49 AM UTC
Posted on May 17, 2011 at 09:49

Can USB_clk pin of STR9 used as GPIO even USB function enable?

and the USB 48MHz is from internal clock!

16-32micros
Associate III
May 17, 2011 7:49 AM UTC
Posted on May 17, 2011 at 09:49

Hi Kuni,

Yes, you can ;) Looking on Table 5 (Device Pin Description) in the STR91xFA datasheet : the default Input/output function of Pin 2.7 is standard GPIO. Hope this clarifies.

STOne-32 :)

[ This message was edited by: STOne-32 on 09-01-2008 13:43 ]