Yes, of course. It can work in the whole range of 3...30V, which is the possible voltage difference between VCC+ and VCC-. It doesn't matter, if it is
- VCC+=0V and VCC-=30V (i.e. working below zero volts) or
- VCC+=30V and VCC-=0V (i.e. working above zero volts) or
- anything between, with the max difference of 30V (absolute max 32V)
Does it answer your question?
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.