Skip to main content
vega
Associate II
Sep 4, 2006 10:38 AM UTC
Question

Can tell me what differences between the UART and the SCI?

Posted on September 04, 2006 at 12:38

Can tell me what differences between the UART and the SCI?

This topic has been closed for replies.

2 replies

vega
vegaAuthor
Associate II
Aug 17, 2006 4:09 AM UTC
Posted on August 17, 2006 at 06:09

I want to know that the UART and the SCI are the same or not.I found some articles to put them together.But if they are the same,why not use the same name.So I want to know what differences between them.Can anyone tell me about the differences of them?

Thank you for helping...

[ This message was edited by: Vega on 17-08-2006 09:40 ]

Viktor POHORELY
ST Employee
Sep 4, 2006 10:38 AM UTC
Posted on September 04, 2006 at 12:38

main difference is the name :)

UART, USART, SCI, ... are different name for same (or similar) things. Why not the same name? Because of (TM) mark on the name...

There could be several differencies in ''special features'' - prescallers, register sets, interrupts, internal structure... but all are compatible and could communicate together.