Skip to main content
rfsingh81
Associate
Aug 29, 2014 6:15 PM UTC
Question

Can't switch LSI to master clock

Posted on August 29, 2014 at 20:15

Hi, I can manage to change clock from HSI>HSE and vice versa. But I am not able to bring LSI as my master clock. Can anyone help please?

I am using STM8S Discovery board and Cosmic C as my compiler.

My code is as follows:

/* MAIN.C file

 * 

 * Copyright (c) 2002-2005 STMicroelectronics

 */

&sharpinclude ''stm8s.h''

u16 c=50000;

u8 i;

main()

{

ErrorStatus status;

CLK_DeInit();

CLK_HSICmd(ENABLE);

while (CLK_GetFlagStatus(CLK_FLAG_HSIRDY)==0);

CLK_LSICmd(ENABLE);

while (CLK_GetFlagStatus(CLK_FLAG_LSIRDY)==0);

CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);

CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV8);

CLK_ClockSwitchCmd(ENABLE);

CLK_CCOConfig(CLK_OUTPUT_MASTER);

CLK_CCOCmd(ENABLE);

GPIO_DeInit (GPIOD);

GPIO_Init (GPIOD,GPIO_PIN_0,GPIO_MODE_OUT_PP_LOW_FAST);

while (1){

// CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER2,ENABLE);

// TIM2_DeInit();

// TIM2_TimeBaseInit(TIM2_PRESCALER_2048, 300);

// TIM2_Cmd(ENABLE);

for(i=0;i<10;i++){

// if (TIM2_GetCounter()>150){

// GPIO_WriteHigh(GPIOD,GPIO_PIN_0);

// }

// else {

// GPIO_WriteLow(GPIOD,GPIO_PIN_0);

// }

while (c>1){

c--;

}

c=50000;

GPIO_WriteReverse(GPIOD,GPIO_PIN_0);

}

status=CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO,CLK_SOURCE_HSE,DISABLE,CLK_CURRENTCLOCKSTATE_ENABLE);

for(i=0;i<10;i++){

// if (TIM2_GetCounter()>150){

// GPIO_WriteHigh(GPIOD,GPIO_PIN_0);

// }

// else {

// GPIO_WriteLow(GPIOD,GPIO_PIN_0);

// }

while (c>1){

c--;

}

c=50000;

GPIO_WriteReverse(GPIOD,GPIO_PIN_0);

}

status=CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO,CLK_SOURCE_LSI,DISABLE,CLK_CURRENTCLOCKSTATE_ENABLE);

}

}

&sharpifdef USE_FULL_ASSERT

/**

  * @brief  Reports the name of the source file and the source line number

  *   where the assert_param error has occurred.

  * @param file: pointer to the source file name

  * @param line: assert_param error line source number

  * @retval None

  */

void assert_failed(uint8_t* file, uint32_t line)

{ 

  /* User can add his own implementation to report the file name and line number,

     ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */

  /* Infinite loop */

  while (1)

  {

  }

}

&sharpendif

#lsi-clock-source
    This topic has been closed for replies.

    1 reply

    Arlet Ottens
    Associate II
    Mar 20, 2017 9:42 AM UTC
    Posted on March 20, 2017 at 10:42

    Make sure the option bytes are set to enable the LSI.  See datasheet for description of option bytes.