Skip to main content
thibaut2
Associate III
Aug 13, 2012 2:15 PM UTC
Question

Can't configure Timer2 configuration registers

Posted on August 13, 2012 at 16:15

Hi.

I'm trying to use Input Capture mode on Timer2 (channel 3) on an STM8S105 (discovery board). It won't work, and when i m watching peripheral registers with appropriated breakpoints, the registers aren't changing from default value.

I m using STVD with cosmic compiler. I'm using firmware libraries. (i already checked out, that every macros was pointing to the right register.)

Here's everything relevant in my code :

    CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER2, ENABLE);

   GPIO_Init(GPIOD, GPIO_PIN_2, GPIO_MODE_IN_PU_NO_IT);

 

    //!\ modify option bytes : select TIMR2-CH3 for AFR1

 

 

    TM2_DISABLE;  //macro resetting CEN bit in TMR2->CR1 register

 

 

    TIM2_DeInit();

 

 

    TIM2_TimeBaseInit(TIM2_PRESCALER_1, 0xFEFE);  // changed from FFFF to FEFE to see if it applies any change to ARR register, and it does not :\

 

   

 

    TIM2_ICInit(TIM2_CHANNEL_3,

 

                 TIM2_ICPOLARITY_FALLING,

 

                 TIM2_ICSELECTION_DIRECTTI,

 

                 TIM2_ICPSC_DIV1,

 

                 0);

 

 

    TIM2_ITConfig(TIM2_IT_CC3, ENABLE);

 

 

    TIM2_CCxCmd(TIM2_CHANNEL_3, ENABLE);

 

    

 

    TM2_ENABLE;    //macro setting CEN bit in TMR2->CR1 register

Has anyone a clue on chat i forgot to enable so this peripheral might work ?
    This topic has been closed for replies.

    2 replies

    thibaut2
    thibaut2Author
    Associate III
    Aug 14, 2012 12:58 PM UTC
    Posted on August 14, 2012 at 14:58

    here a more precise example :

    TIM2->CR1 |= (uint8_t)TIM2_CR1_CEN;

    after this instruction i shall see register of TIM2-CR1 (address 0x5300) change from 0x00 to 0x01.

    But it won't work... and i already checked base_address, macros, ref manual, and peripheral registers, they re all pointing to the same address 0x5300.

    My clock is also enable. I'm using HSI as main clock.

    thibaut2
    thibaut2Author
    Associate III
    Aug 14, 2012 1:39 PM UTC
    Posted on August 14, 2012 at 15:39

    I finally found it, my mistake :\

    i was enabling/disabling every peripheral clock, but i had kept timer5 and 6 whereas they re not on STM8S105, and timer5 and 2 share same adress. So disabling timer5 was disabling my clock....

    Dumb mistake ...