Skip to main content
dvir
Associate III
May 21, 2006 4:21 AM UTC
Question

CAN .sre file for ST10f276

Posted on May 21, 2006 at 06:21

CAN .sre file for ST10f276

This topic has been closed for replies.

3 replies

dvir
dvirAuthor
Associate III
May 18, 2006 2:09 AM UTC
Posted on May 18, 2006 at 04:09

Hello,

does anyone know where can i get a sre file for TASKING's CrossView to work with the ST10f276 using ROM-MONITOR through the CAN or the second serial port (XASC) ?

thanks in advance,

Dvir :(

najoua
Associate
May 18, 2006 8:55 AM UTC
Posted on May 18, 2006 at 10:55

Hello Dvir,

To use the second serial port, you can modify the files c166\mon\serial.c and serial.h accordingly.

By default, serial port 0 is defined by macro ''PORT'' in file mondef.h.

To rebuild the ST10276 monitor, goto directory ''c166\mon\mon167'' and run from the command line:

c166\bin\mk166 clean

c166\bin\mk166

To use the rebuilt monitor, copy file m167r.sre to your project directory.

For more details and clarifications, you can contact TASKING technical support.

I hope this helps you,

With best regards,

Najoua.

dvir
dvirAuthor
Associate III
May 21, 2006 4:21 AM UTC
Posted on May 21, 2006 at 06:21

hello Najoua,

thanks for your help, but i was looking for an already made and tested sre file.

As for Tasking support, they said they don't have the time to write this sre just for one customer.

thanks and best regards,

Dvir