Visitor II
Apr 10, 2012 1:31 PM UTC
Question
CAN Bus
- 1 reply
- 1077 views
Posted on April 10, 2012 at 15:31
I try to use an exemple by KEIL, but when i try to debug it doesn't work,
my main is : ''/******************** (C) COPYRIGHT 2007 STMicroelectronics ******************** * File Name : main.c * Author : MCD Application Team * Version : V2.0 * Date : 12/07/2007 * Description : Main program body ******************************************************************************** * THE PRESENT SOFTWARE WHICH IS FOR GUIDANCE ONLY AIMS AT PROVIDING CUSTOMERS WITH * CODING INFORMATION REGARDING THEIR PRODUCTS IN ORDER FOR THEM TO SAVE TIME. AS * A RESULT, STMICROELECTRONICS SHALL NOT BE HELD LIABLE FOR ANY DIRECT, INDIRECT * OR CONSEQUENTIAL DAMAGES WITH RESPECT TO ANY CLAIMS ARISING FROM THE CONTENT * OF SUCH SOFTWARE AND/OR THE USE MADE BY CUSTOMERS OF THE CODING INFORMATION * CONTAINED HEREIN IN CONNECTION WITH THEIR PRODUCTS. *******************************************************************************/ /* Standard include ----------------------------------------------------------*/ #include ''91x_lib.h'' /* Include of other module interface headers ---------------------------------*/ /* Local includes ------------------------------------------------------------*/ /* Private typedef -----------------------------------------------------------*/ /* Private define ------------------------------------------------------------*/ /* Private macro -------------------------------------------------------------*/ /* Private variables ---------------------------------------------------------*/ canmsg RxCanMsg; canmsg CanMsg; GPIO_InitTypeDef GPIO_InitStructure; CAN_InitTypeDef CAN_InitStructure; /* buffer for receive messages */ canmsg RxCanMsg; /* used message object numbers */ enum { CAN_TX_MSGOBJ = 0, CAN_RX_MSGOBJ = 1 }; /* array of pre-defined transmit messages */ canmsg TxCanMsg[3] = { { CAN_STD_ID, 0x123, 4, { 0x01, 0x02, 0x04, 0x08 } }, { CAN_STD_ID, 0x321, 4, { 0xAA, 0x55, 0xAA, 0x55 } }, { CAN_EXT_ID, 0x12345678, 8, { 0x10, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16, 0x17 } } }; /* Private functions ---------------------------------------------------------*/ void SCU_Configuration(void) { SCU_MCLKSourceConfig(SCU_MCLK_OSC); SCU_PCLKDivisorConfig(SCU_PCLK_Div2); SCU_PLLFactorsConfig(128,25,4); SCU_PLLCmd(ENABLE); SCU_MCLKSourceConfig(SCU_MCLK_PLL); SCU_APBPeriphClockConfig(__CAN, ENABLE); SCU_APBPeriphClockConfig(__GPIO0, ENABLE); SCU_APBPeriphClockConfig(__GPIO1, ENABLE); SCU_APBPeriphClockConfig(__GPIO3, ENABLE); SCU_APBPeriphClockConfig(__GPIO5, ENABLE); SCU_APBPeriphClockConfig(__GPIO9, ENABLE); SCU_AHBPeriphClockConfig(__VIC, ENABLE); SCU_APBPeriphReset(__CAN, DISABLE); SCU_APBPeriphReset(__GPIO0, DISABLE); SCU_APBPeriphReset(__GPIO1, DISABLE); SCU_APBPeriphReset(__GPIO3, DISABLE); SCU_APBPeriphReset(__GPIO5, DISABLE); SCU_APBPeriphReset(__GPIO9, DISABLE); SCU_AHBPeriphReset(__VIC, DISABLE); } void IO_Init(void) { /* P5.0 alternate input 1, CAN_RX pin 12*/ GPIO_StructInit(&GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin=GPIO_Pin_0; GPIO_InitStructure.GPIO_Direction=GPIO_PinInput; GPIO_InitStructure.GPIO_IPInputConnected=GPIO_IPInputConnected_Enable; GPIO_InitStructure.GPIO_Alternate=GPIO_InputAlt1; GPIO_Init(GPIO5,&GPIO_InitStructure); /* P5.0 alternate output 2, CAN_TX */ GPIO_StructInit(&GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin=GPIO_Pin_0; GPIO_InitStructure.GPIO_Direction=GPIO_PinOutput; GPIO_InitStructure.GPIO_Type=GPIO_Type_PushPull; GPIO_InitStructure.GPIO_IPInputConnected=GPIO_IPInputConnected_Disable; GPIO_InitStructure.GPIO_Alternate=GPIO_OutputAlt2; GPIO_Init(GPIO5,&GPIO_InitStructure); } void CAN_Com_LoopBack(void) { /* initialize the CAN at a standard bitrate, interrupts disabled */ CAN_InitStructure.CAN_ConfigParameters=0x0; CAN_InitStructure.CAN_Bitrate=CAN_BITRATE_1M; CAN_Init(&CAN_InitStructure); /* switch into Loopback+Silent mode (self-test) */ CAN_EnterTestMode(CAN_TESTR_LBACK | CAN_TESTR_SILENT); /* configure the message objects */ CAN_SetUnusedAllMsgObj(); CAN_SetTxMsgObj(CAN_TX_MSGOBJ, CAN_STD_ID, DISABLE); CAN_SetRxMsgObj(CAN_RX_MSGOBJ, CAN_STD_ID, 0, CAN_LAST_STD_ID, TRUE); /* Send the pre-defined answer */ CAN_SendMessage(CAN_TX_MSGOBJ, &TxCanMsg[1]); /* wait until end of transmission */ CAN_WaitEndOfTx(); /* wait for reception of a data frame */ while (!CAN_ReceiveMessage(CAN_RX_MSGOBJ, FALSE, &RxCanMsg)) { /*Add Timer*/ } /* Test Received Msg */ if((RxCanMsg.IdType == CAN_STD_ID)&&(RxCanMsg.Id == 0x321)&&(RxCanMsg.Dlc == 4) &&(RxCanMsg.Data[0]==0xAA)&&(RxCanMsg.Data[1]==0x55)&&(RxCanMsg.Data[2]==0xAA)&&(RxCanMsg.Data[3]==0x55)){ /*Received Msg OK*/ } else { /*Received Msg KO*/ } /* release the message objects */ CAN_ReleaseTxMessage(CAN_TX_MSGOBJ); CAN_ReleaseRxMessage(CAN_RX_MSGOBJ); /* switch back into Normal mode */ CAN_LeaveTestMode(); } /******************************************************************************* * Function Name : main * Description : Main program * Input : None * Output : None * Return : None *******************************************************************************/ int main(void) { SCU_Configuration();/*PCLK=8MHz*/ IO_Init(); /* CAN tests */ CAN_Com_LoopBack();/* send and receive some frame */ while(1); } /******************* (C) COPYRIGHT 2007 STMicroelectronics *****END OF FILE****/ '' you can see my debug results in the attach file Best regards