Skip to main content
MQi.1
Senior II
March 28, 2020
Question

Can assembly code running on stm8s-dicovery board?

I have tested my stm8s-discovery board for 2 days. The MCU is stm8s105c6t6, the Hex format file produced in c language on the IAR EW platform, could run as expected when uploaded into the board, but the final file from assembly language, both in Hex and .s19 format, generated from STVD, cann't run at all when uploading.

I have tested download code from STVD and STVP, in format of intel hex, intel hex extended, and motorola s19, neither of it could run.

So, my question is, whether file produced in assembly code could run on stm8s105c6t6? Is there any other configuration option, or due to ST-LINK(v2) or stms8-dicovery board itself?

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    March 28, 2020

    The problem would seem to be with WHAT you're loading, not how it is packaged/formatted. The output of the C compiler is machine code.

    Perhaps review more critically what you're generating out of the assembler/linker, look at the listing files, map files, and expectations the micro-controller has for starting and executing code. Perhaps disassemble the working code to better understand its structure.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    MQi.1
    MQi.1Author
    Senior II
    March 30, 2020

    My code is here:

    stm8/

       #include "mapping.inc"

       segment 'rom'

    SET

       bset $5002, #3

       bset $5002, #4

       bset $5002, #5

       bset $5002, #6

    LOOP

       bset $5000, #3

       bset $5000, #4

       bset $5000, #5

       bset $5000, #6

       ;bcpl $5000, #5

       ;bcpl $5000, #6

       ;jra LOOP

       ;jra DELAY_1

       ;bcpl $5000, #3

       ;bcpl $5000, #4

       ;bcpl $5000, #5

       ;bcpl $5000, #6

       ;jra DELAY_1

       jra LOOP

       END

    Is it lack of anything?

    YAY.1
    Senior
    August 22, 2020

    Which program do you use to programming ?

    Unfortunately,

    I dont know stm8 programing with assembly language.

    But,

    If you dont use ST-LINK/V2 in-circuit debugger/programmer for STM8 and STM32, Could you try with this again ?

    And

    you should update firmware....

    and

    it is seeing that somethings is mising.

    You may not have specified ram location,stack or something

    (stm32 example)

        PUBLIC __vector_table

        SECTION .text:CODE:REORDER(10)

        REQUIRE __vector_table

        SECTION CSTACK:DATA:NOROOT(10)

        SECTION .intvec:CODE:NOROOT(10)

        DATA

    __vector_table

        DCD   sfe(CSTACK)

        DCD   SETUP

        SECTION .text:CODE:REORDER:NOROOT(10)

        THUMB

    I hope this will help you.

    MQi.1
    MQi.1Author
    Senior II
    August 24, 2020

    Thanks, I will try it later.