Skip to main content
yourmom
Associate
February 23, 2004
Question

Can anyone spot the bug?

  • February 23, 2004
  • 2 replies
  • 754 views
Posted on February 23, 2004 at 08:23

Can anyone spot the bug?

This topic has been closed for replies.

2 replies

yourmom
yourmomAuthor
Associate
February 23, 2004
Posted on February 23, 2004 at 03:08

Can anyone see a bug in this code which would allow the stack pointer to be modified?

ROM:8A30 WRITETOEEPROMX: ; CODE XREF: WRITEATOEEFROMX+9j

ROM:8A30 ; WRITEATOEEFROMX+Ej ...

ROM:8A30 83 trap

ROM:8A31 CD 82 23 call ENABLEINTERRUPTS

ROM:8A34 AD 0D callr KILLWRITEOKBITS

ROM:8A34 ; End of function WRITEATOEEFROMX

ROM:8A34

ROM:8A36

ROM:8A36 ; ¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦ S U B R O U T I N E ¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦

ROM:8A36

ROM:8A36

ROM:8A36 EECONTEXTRESTR: ; CODE XREF: WRITEATOEEFROMX+17p

ROM:8A36 ; WRITEATOEEFROMX+1Cp ...

ROM:8A36 B6 72 ld a, EESAVERCADRH

ROM:8A38 B7 4A ld RC1ADDRH, a

ROM:8A3A B6 73 ld a, EESAVERCADRL

ROM:8A3C B7 4B ld RC1ADDRL, a

ROM:8A3E B6 70 ld a, SW1

ROM:8A40 BE 71 ld x, SW2

ROM:8A42 81 ret

ROM:46A0 SMOD3JMPXA: ; CODE XREF: SETUPBLOCKOUT+1p

ROM:46A0 3F 5E clr NUMINFOBYTES ; Init # bytes in info field

ROM:46A2 3F 5F clr INFOFIELDPTR ; Init pointer into info field

ROM:46A4 CF 01 A5 ld SELDMOD3_01, x ; Save address of routine that will

ROM:46A7 C7 01 A6 ld SELDMOD3_02, a ; build the output message

ROM:46AA A6 5A ld a, #$5A ; Get a JMP $XXXX instruction

ROM:46AC C7 01 A4 ld SELDMOD3_00, a ; at SELFMOD3

ROM:46AF 3F 61 clr MSGOUTPTR ; Clear pointer to current byte #

ROM:46B1 05 50 0A btjf FLAGS0, #2, loc_0_46BE

ROM:46B4 CD 46 0C call BUILDMSGFROMSM3

ROM:46B7 10 0B bset UARTREG, #0

ROM:46B9 CD 82 23 call ENABLEINTERRUPTS

ROM:46BC 9A rim

ROM:46BD 81 ret

ROM:46BE ; ---------------------------------------------------------------------------
kr_it
Visitor II
February 23, 2004
Posted on February 23, 2004 at 08:23

Hi!

Can you check your stack depth at each of your calling function, for example check at ''call ENABLEINTERRUPTS'' and so on, because if your stack size is nearing the limit and if you are using the stack(i.e. calling function), then it may cause a problem.

Also check the no of called functions inside a function.

Like if function1 calling function2 and this calling function3 and so on.

--Krsel