Skip to main content
mkruger
Associate
Nov 17, 2009 3:28 PM UTC
Question

Bulk erase bootloader command via SPI

Posted on November 17, 2009 at 16:28

Bulk erase bootloader command via SPI

    This topic has been closed for replies.

    2 replies

    mkruger
    mkrugerAuthor
    Associate
    May 17, 2011 1:05 PM UTC
    Posted on May 17, 2011 at 15:05

    *Comic slap to the forehead*

    Argh. Order of operations issue. Should probably load the bootloader write/erase routines prior to trying to erase something. Duh! I need more sleep apparently.

    mkruger
    mkrugerAuthor
    Associate
    May 17, 2011 1:05 PM UTC
    Posted on May 17, 2011 at 15:05

    STM8S105C6

    I am trying to bulk erase the part via SPI using the precompiled bootloader write/erase routines provided by ST. I am able to write memory locations without issue, so I am fairly certain the SPI transactions are properly set up (though there is always room for error). Here is the code:

    {

    tUBYTE Request[4];

    tUBYTE Response[4];

    tUBYTE AckByte[2];

    Request[0] = 0x7F;//SYNCHR Byte

    Request[1] = 0x80;//NSYNCHR Byte

    DigitalOutSetDigitalState(dHAL_DO_RESET_SECOND_MICRO, dINACTIVE);

    SleepMs(10);

    DigitalOutSetDigitalState(dHAL_DO_RESET_SECOND_MICRO, dACTIVE);

    SleepMs(5);

    SpiTransaction(&Request[0], &Response[0], 2); // Put ST into boot mode

    Request[0] = 0x43; // Erase command

    Request[1] = 0xBC; // compliment

    SpiTransaction(&Request[0], &Response[0], 2); // 2 bytes sent

    SpiTransaction(&AckByte[0], &AckByte[0], 1); // 1 byte sent

    if(AckByte[0] == 0x79) // ASCII 'y'

    {

    Request[2] = 0xFF; // Total erase code

    Request[3] = 0x00; // compliment

    SpiTransaction(&Request[2], &Response[2], 2); // 2 bytes sent

    SleepMs(500); // 500 millisecond delay

    SpiTransaction(&AckByte[1], &AckByte[1], 1); // 1 byte sent

    if(AckByte[1] == 0x79) // ASCII 'y'

    return(eTRUE); // Success

    }

    return(eFALSE); // Failure

    }

    I receive the ACK after the 500ms delay but when I cycle power, the application code has not been erased. Anyone see any glaringly obvious mistakes?