Skip to main content
dcramer
Associate II
March 20, 2008
Question

Bootloader for STR912

  • March 20, 2008
  • 11 replies
  • 2196 views
Posted on March 20, 2008 at 15:07

Bootloader for STR912

This topic has been closed for replies.

11 replies

dcramer
dcramerAuthor
Associate II
May 17, 2011
Posted on May 17, 2011 at 09:50

I am trying to load a bootloader into Bank 1. I used Segger JLinkSTR91x.exe to set the default boot bank to 1, then I downloaded my code with IAR Embedded WorkBench 4.42. I then examined my memory with JMem.exe. Only the first sector from address 0 to 0x1fff contains my code. The code and data should go to 0x705b. If I load the code to bank 0, it will all load. Why is the code stop loading after the first sector in bank 1.

TIA

jilisegiar
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:50

Which flash loader are using to load your code into Bank1

jilisegiar
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:50

open

Project->options->debugger->Download

to see which flash loader you are using.

dcramer
dcramerAuthor
Associate II
May 17, 2011
Posted on May 17, 2011 at 09:50

I am using the workbench and loading it in debug mode.

jilisegiar
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:50

@elai and @dcramer:

try to perform full chip erase using JlinkSTR91x.exe then try aging what you did.

enricol
Associate II
May 17, 2011
Posted on May 17, 2011 at 09:50

I am trying to understand the sample bootloader provided by ST as I need to port it from IAR to RIDE7(gcc) environment. To begin, I tried to write a simple blinking LED application and load it into Flash Bank 1, but failed...

Here is how I did it:

1) Erase the chip using JFlashARM.exe

2) Set default boot bank to 1 using Segger JLinkSTR91x.exe

3) Program the .hex file into the board using JFlashARM.exe

I got the following errors:

Programming failed @ address 0x00002000 (Algo13: Sector is locked)

 

Failed to program target

But if I set the boot bank back to 0, erase, and program, I won't get the error... why is that?

Any help/hint would be greatly appreciated!

Thanks

:-Y

[ This message was edited by: elai on 05-03-2008 23:19 ]

dcramer
dcramerAuthor
Associate II
May 17, 2011
Posted on May 17, 2011 at 09:50

I am using FlashSTR91x.d79 for the flash downloader.

jilisegiar
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:50

Hi,

The new version of segger tools(V3.80) supports the 2 banks 0 & 1.

http://www.segger.com/download_jlink.html

Rgds

jmullens
Associate II
May 17, 2011
Posted on May 17, 2011 at 09:50

I was stuck here with this as well. My first nonideal solution was to use my own application to write to bank1 in the flash. When I switched banks using the Segger programmer, and used the Jflash utility to read back the memory, I would sometimes get odd behavior. I don't know how much I can trust the Segger J-flash (v3.78D), when running in bank1-boot mode. When I mapped the device to bank1, and read back the memory, I got the repeat of my bios code [0x0:0x79B7], in 0x8000, 0x10000,0x18000,0x20000, etc..

I have working applications in both Bank0 and Bank1, and know this memory display was bogus.

I decided to try my luck with the HiTop debugger/Tantino-Jtag . I had the IAR (4.41A) compiler generate an .ELF file that I imported into the debugger. There is an option to choose that the bootbank will be. With a little bit of setup to specify the the Ram start address (0x4000000), the flash type,''STR9xF44_Bank1'', and the ''CSx Mapping - CS0 is mapped to the secondary flash, CS1 to main flash'', I was able to load and debug my code in bank1.

Anecdotally, I was told that because the processor still generated interrupts after it was reset, this confused a lot of Jtag programmers.

Hitex got around this by creating a Startup-script. I subsequently modified this to reflect the boot-bank remapping. I've included this file that needs to be renamed with the extension ''.scr''

I had to change the 91x_init.s file supplied with the USB and Ethernet download examples for bank1 operation and add the line:

LDR R6, =0x54000000

LDR R7, =0x0

STR R7, [R6]

Before these other lines:

LDR R6, =0x54000004 ; non boot bank size

LDR R7, =0x6 ; 512K

STR R7, [R6]

LDR R6, =0x5400000C ; boot bank address = Bank 1

LDR R7, =0x0 ; 0x0

STR R7, [R6]

LDR R6, =0x54000010 ; non boot bank address = Bank 0

LDR R7, =0x20000 ; 0x10000 = 4x 0x4000

STR R7, [R6]

LDR R6, =0x54000018 ; enable Non Boot bank

LDR R7, =0x18

STR R7, [R6]

Without it, my code did not work . Also, adding the IAR compiler intrinsic function __ramfunc() to the beginning of FMI_Config() in the 91x_fmi.c library, made this function work by after I remapped the flash.

You must also make sure that you linker file, lnkarm_flash.xcl, beings at

-DROMSTART=0x0

-DROMEND =0x7FFF

enricol
Associate II
May 17, 2011
Posted on May 17, 2011 at 09:50

Hi jilisegiar,

I tried erasing the chip using JlinkSTR91.exe according to:

http://null

1) Perform full chip erase.

Code:

Connecting to STR9: O.K.

J-Link>erase 0,ffffffff

Erasing flash...

J-Link>showconf

Reading flash configuration register...

ISC-CONFIGURATION: 0x0000-0000-0000-0000

Bit 0 = 0: Flash Bank 0 sector is not protec

Bit 1 = 0: Flash Bank 0 sector is not protec

Bit 2 = 0: Flash Bank 0 sector is not protec

Bit 3 = 0: Flash Bank 0 sector is not protec

Bit 4 = 0: Flash Bank 0 sector is not protec

Bit 5 = 0: Flash Bank 0 sector is not protec

Bit 6 = 0: Flash Bank 0 sector is not protec

Bit 7 = 0: Flash Bank 0 sector is not protec

Bit 32 = 0: Flash Bank 1 sector is not prote

Bit 33 = 0: Flash Bank 1 sector is not prote

Bit 34 = 0: Flash Bank 1 sector is not prote

Bit 35 = 0: Flash Bank 1 sector is not prote

Bit 48 = 0: CS 0 is mapped to main flash.

Bit 49 = 0: LVD_th The LVD threshold is set

Bit 50 = 0: LVD_RESET_SELECT LVD Reset Out i

Bit 51 = 0: LVD_WARNING_SELECT Early Warning

Bit 63 = 0: Lock Bit Write to unprogrammed O

J-Link>blank

Sector 0 (Flash 0): is blank

Sector 1 (Flash 0): is blank

Sector 2 (Flash 0): is blank

Sector 3 (Flash 0): is blank

Sector 4 (Flash 0): is blank

Sector 5 (Flash 0): is blank

Sector 6 (Flash 0): is blank

Sector 7 (Flash 0): is blank

Sector 32 (Flash 1): is blank

Sector 33 (Flash 1): is blank

Sector 34 (Flash 1): is blank

Sector 35 (Flash 1): is blank

Sector 49 (Configuration sector): is blank

Sector 50 (User-Code): is blank

Sector 51 (OTP Sector): is not blank

2) Set Boot Bank to Bank 1:

Code:

J-Link>setb 1

Writing flash configuration register...

Writing O.K. CS1 is set to main flash.

J-Link>showconf

Reading flash configuration register...

ISC-CONFIGURATION: 0x0001-0000-0000-0000

Bit 0 = 0: Flash Bank 0 sector is not protected.

Bit 1 = 0: Flash Bank 0 sector is not protected.

Bit 2 = 0: Flash Bank 0 sector is not protected.

Bit 3 = 0: Flash Bank 0 sector is not protected.

Bit 4 = 0: Flash Bank 0 sector is not protected.

Bit 5 = 0: Flash Bank 0 sector is not protected.

Bit 6 = 0: Flash Bank 0 sector is not protected.

Bit 7 = 0: Flash Bank 0 sector is not protected.

Bit 32 = 0: Flash Bank 1 sector is not protected.

Bit 33 = 0: Flash Bank 1 sector is not protected.

Bit 34 = 0: Flash Bank 1 sector is not protected.

Bit 35 = 0: Flash Bank 1 sector is not protected.

Bit 48 = 1: CS 1 is mapped to main flash

Bit 49 = 0: LVD_th The LVD threshold is set to 2.4 V.

Bit 50 = 0: LVD_RESET_SELECT LVD Reset Out is generated by VDD input onl

Bit 51 = 0: LVD_WARNING_SELECT Early Warning is generated by VDD input o

Bit 63 = 0: Lock Bit Write to unprogrammed OTP location is allowed.

J-Link>blank

Sector 0 (Flash 0): is blank

Sector 1 (Flash 0): is blank

Sector 2 (Flash 0): is blank

Sector 3 (Flash 0): is blank

Sector 4 (Flash 0): is blank

Sector 5 (Flash 0): is blank

Sector 6 (Flash 0): is blank

Sector 7 (Flash 0): is blank

Sector 32 (Flash 1): is blank

Sector 33 (Flash 1): is blank

Sector 34 (Flash 1): is blank

Sector 35 (Flash 1): is blank

Sector 49 (Configuration sector): is not blank

Sector 50 (User-Code): is blank

Sector 51 (OTP Sector): is not blank

J-Link> q

3) Now Open JFlashARM.exe and program the .hex file

and still getting the same error message