Skip to main content
slim2
Associate
Sep 25, 2006 6:33 AM UTC
Question

BOOT

Posted on September 25, 2006 at 08:33

BOOT

This topic has been closed for replies.

2 replies

slim2
slim2Author
Associate
Apr 16, 2004 9:54 AM UTC
Posted on April 16, 2004 at 11:54

TQFP64 package pin 7 is BOOTEN. Does it have any meaning for TQFP64

Can I use pulldown resistor for BOOTEN and forget this pin ? Or is it used for programming ?
sany_as
Associate II
Sep 23, 2006 4:13 AM UTC
Posted on September 23, 2006 at 06:13

Sir,

we are developing our project in the ST development board STDV710.

We want to boot our progrmme from internal flash/RAM. As per the datasheet, in this case we have to use

BOOTEN BOOT0 BOOT1 MEMORY

0 X X FLASH

1 0 0 FLASH

1 1 0 RAM

in that case can we use the (BOOT0)U0Tx and (BOOT1)U1Tx IN THE UART MODE.