Skip to main content
infiniium
Associate
Apr 19, 2011 7:39 PM UTC
Question

Beep function with STM8L Discovery

Posted on April 19, 2011 at 21:39

Hello,

I want to use the beep function with my STM8L Discovery.

After writing the program to STM8L, I connect the a piezo speaker between PA0 and GND.

The program is as following:

// Initialize

    BEEP_LSICalibrationConfig(16000000);

    BEEP_Init(BEEP_Frequency_1KHz);

//Beep

    BEEP_Cmd(ENABLE);

    delay_ms(200);

    BEEP_Cmd(DISABLE);

But it doesn't work.

Do I need something another command on Initialization process ?

I know the PA0 is connected to the SWIM. Is it affect something bad for the beeper function?
    This topic has been closed for replies.

    1 reply

    lowpowermcu
    Associate III
    Jun 1, 2011 9:46 AM UTC
    Posted on June 01, 2011 at 11:46

    Perhaps you need something like this:

    CLK_PeripheralClockConfig(CLK_Peripheral_BEEP, ENABLE);