Skip to main content
danielcatina9
Associate
Jan 15, 2007 5:11 AM UTC
Question

basic EMI Interface question

Posted on January 15, 2007 at 06:11

basic EMI Interface question

This topic has been closed for replies.

2 replies

sjo
Associate III
May 17, 2011 7:35 AM UTC
Posted on May 17, 2011 at 09:35

Depends on the device you are connecting to.

Most Flash/SRAMS will require the external latches as they do not support multiplexed addressing.

The datasheet of the part you are using will tell you what mode it supports.

Regards

sjo

danielcatina9
Associate
May 17, 2011 7:35 AM UTC
Posted on May 17, 2011 at 09:35

Do I need to add an external latch in order to interface the processor to a 1Mx16 SRAM chip?. I know is a basic question, but it seems that the documentation I'm reading suggests that an external latch is not needed: based on ''Insider's guide'' by Hitex (p.54) or on the reference manual (p.37. ''Mux mode with 16-bit data, 24-bit address'')