Skip to main content
manuel239955_st
Visitor II
Jan 8, 2016 1:06 PM UTC
Question

attach only stm8

Posted on January 08, 2016 at 14:06

is it possible with the stvd to attach / connect only to a already running target via swim?

#swim #stm8 #attach
    This topic has been closed for replies.

    1 reply

    Philipp Krause
    Senior II
    Jan 13, 2016 12:13 PM UTC
    Posted on January 13, 2016 at 13:13

    I'm not using STVD, but in general, STVD is more complete than the free tools. With the free stm8flash, I can attach to a running target to write a new program into the flash memory via ST-Link or ST-Link/v2 anytime. So I guess it will work fine with STVD.

    Philipp