Skip to main content
flankerus
Associate II
Aug 3, 2018 9:39 AM UTC
Question

ASM, error on copy segment 'code>ram'

I'm trying to compile an example from "ST Aseembler Linker", Chapter 4.4 "Segmentation"

stm8/
	segment byte at: 0 'code'
	segment byte at: 8000 'ram'
	segment 'ram>code'
	
label1: nop
	
	end

and i get the following error:

Error in map file Debug\00_test.map: wrong map file format: can't find segment type!

 The command: "abslist Debug\main.lsr -exe Debug\00_test.s19" has failed, the returned value is: 1

exit code=1.

file 00_test.map has next contains:

Segment List
------------
 
c:\users\flanker\documents\stvd\00_test\main.asm[3] 4- 7 0 - 0 'code'
c:\users\flanker\documents\stvd\00_test\main.asm[4] 4- 7 8000 - 8000 'ram' [text]
 
 
Class List
----------
 
0 ' code' byte from 0 to 0 (lim FFFFFFFF) = 0% D
0 ' ram' byte from 8000 to 8000 (lim FFFFFFFF) = 0% C
 
 
 
External Label list
-------------------
 
Symbol Name Value Scope Def(line)
 
 
0 labels

What am I doing wrong?

Thanks!

    This topic has been closed for replies.