Skip to main content
PhilippeSIMIER
Associate II
October 5, 2022
Question

application note AN3281 to implement the I2C bus for the STM8S microcontroller.

You have published an application note AN3281 to implement the I2C bus.

Where can we download the example programs described in the note?

Thank you for your answers

This topic has been closed for replies.

6 replies

Peter BENSCH
ST Technical Moderator
October 5, 2022

You can find it on the website of the STSW-STM8004.

Good luck!

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PhilippeSIMIER
Associate II
October 5, 2022

Thanks

Peter BENSCH
ST Technical Moderator
October 5, 2022

You're welcome!

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PhilippeSIMIER
Associate II
October 5, 2022

I managed to download the program. Thanks.

Have you released an equivalent that uses the SPL library?

Regards

Peter BENSCH
ST Technical Moderator
October 5, 2022

The program for the AN3281 was developed many years before the SPL and represents, so to speak, a first approach to working with I2C on the STM8.

However, the SPL has since supported all functions of the I2C peripheral in the STM8, so the AN3281 should only be considered as a reference.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PhilippeSIMIER
Associate II
October 5, 2022

My issue is the following :

I use the nucleo_8s207k8 evaluation kit.

I am trying to enable I2C bus as master with these functions

void clock_setup(void) {
 
 CLK_DeInit();
 
 CLK_HSECmd(DISABLE);
 CLK_LSICmd(DISABLE);
 CLK_HSICmd(ENABLE);
 while (CLK_GetFlagStatus(CLK_FLAG_HSIRDY) == FALSE);
 
 
 CLK_ClockSwitchCmd(ENABLE);
 CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1); // HSI à 16 MHz
 CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1); // soit CPU à 16Mhz
 
 CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSI,
 DISABLE, CLK_CURRENTCLOCKSTATE_ENABLE);
 
 CLK_PeripheralClockConfig(CLK_PERIPHERAL_SPI, DISABLE);
 CLK_PeripheralClockConfig(CLK_PERIPHERAL_I2C, ENABLE);
 CLK_PeripheralClockConfig(CLK_PERIPHERAL_ADC, DISABLE);
 CLK_PeripheralClockConfig(CLK_PERIPHERAL_AWU, DISABLE);
 CLK_PeripheralClockConfig(CLK_PERIPHERAL_UART1, DISABLE);
 CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER1, DISABLE);
 CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER2, DISABLE);
 CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER4, DISABLE);
}
 
void GPIO_setup(void) {
 GPIO_DeInit(GPIOB);
 GPIO_Init(GPIOB, GPIO_PIN_4, GPIO_MODE_OUT_OD_HIZ_FAST);
 GPIO_Init(GPIOB, GPIO_PIN_5, GPIO_MODE_OUT_OD_HIZ_FAST);
 GPIO_WriteHigh(GPIOB, GPIO_PIN_4);
 GPIO_WriteHigh(GPIOB, GPIO_PIN_5);
}
 
void I2C_setup(void) {
 I2C_DeInit();
 I2C_Init(10000,
 BH1750_addr,
 I2C_DUTYCYCLE_2,
 I2C_ACK_CURR,
 I2C_ADDMODE_7BIT,
 16);
 
 I2C_Cmd(ENABLE);
}

However the I2C_FLAG_BUSBUSY remains at logical true

Why ?

 uint16_t time_out = 5000;
 
 /* If I2C bus is busy wait until it is free */
 while (I2C_GetFlagStatus(I2C_FLAG_BUSBUSY)&& (--time_out));
 if (!time_out) return 1;

Do you have an explanation ?

regards

Philippe S Teacher