Skip to main content
vandykel
Associate
July 11, 2003
Question

Anyone gotten xfree_4.zip and gdk14.zip to work with XFree86 4.x.x on Consumer?

  • July 11, 2003
  • 1 reply
  • 588 views
Posted on July 11, 2003 at 12:52

Anyone gotten xfree_4.zip and gdk14.zip to work with XFree86 4.x.x on Consumer?

This topic has been closed for replies.

1 reply

vandykel
vandykelAuthor
Associate
July 11, 2003
Posted on July 11, 2003 at 12:52

I have tried to use the gdk14 and xfree_4.zip with XFree86 4.2.0 for

the STPC Consumer platform.

However I have a PCI configuration and the stpc_driver.c uses ISA

probes. Furthermore the xfree4.a supplied by xfree_4.zip is not

reproducible, thus far, using the gdk14 source base. The gdk14

supplied buildlib, in the linux project, does not produce the same

object when modified to match the .o's found in xfree4.a .

I have just found the stpckit which has the same stpc_driver.c (with

the dos line feeds stripped). This will be tried next.

Has anyone successfully used these libraries to produce X 4.x.x for the stpc

consumer?