Skip to main content
hg-chen
Associate III
Apr 26, 2007 4:47 AM UTC
Question

any UART sample code runs on STR711-SK/IAR?

Posted on April 26, 2007 at 06:47

any UART sample code runs on STR711-SK/IAR?

This topic has been closed for replies.

4 replies

hg-chen
hg-chenAuthor
Associate III
Apr 23, 2007 6:40 AM UTC
Posted on April 23, 2007 at 08:40

Does anyone get UART sample code runs on STR711-SK/IAR?

not on STR710-EVAL!

hg-chen
hg-chenAuthor
Associate III
Apr 23, 2007 7:33 AM UTC
Posted on April 23, 2007 at 09:33

There are examples in directory C:\....\ARM\examples\ST\STR71x\STR71xLibrary\examples\uart

but the example seems to use UART0, but the STR711-SK/IAR board 2 UART ports are UART1 and UART2? the code is not match with the hardware?

and what can I see if the UART works? via Hyperterminal?

what message I can see?

hg-chen
hg-chenAuthor
Associate III
Apr 23, 2007 7:52 AM UTC
Posted on April 23, 2007 at 09:52

I see the UARTx is selected by jumpers!

another question is can I use the program for baud rate higher than 9600? how to do it?

hg-chen
hg-chenAuthor
Associate III
Apr 23, 2007 9:39 PM UTC
Posted on April 23, 2007 at 23:39

thank you,

It works in UART polling sample code!

in bps 9600 , the hyperterminal responds characters as I typed!

But when I configure as 19200, the hyperterminal responds data not as I typed, for example, I press ''Enter'' 4 times, the hyperterminal responds as 2 question mark ''? ?'' !?

anything wrong?