Skip to main content
Lightning Stalker
Visitor II
Oct 23, 2017 8:53 AM UTC
Question

Any plans for low pin-count STM8L devices?

Posted on October 23, 2017 at 10:53

Occasionally we have need for a 6, 8, or 14-pin MCU.  For instance SOT23-6 or leadless devices to conserve board space.  Up until now, PIC10 and ATtiny have been the only choices, but it's good to have some other options.  The STM8L's 12-bit ADC, DAC, and 16-bit PWM would be particularly useful.  So can we expect to see a low pin-count STM8L sometime in the future?

#low-power #future #stm8 #battery-life
This topic has been closed for replies.

5 replies

Simon V.
ST Employee
Oct 23, 2017 9:10 AM UTC
Posted on October 23, 2017 at 11:10

Hello,

Thank you for your question.

For the moment the smallest STM8 package is SO8 with STM8S001J3 reference.

Product link :

http://www.st.com/en/microcontrollers/stm8s001j3.html

 

Regards,

Simon

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Philipp Krause
Senior II
Oct 23, 2017 10:20 AM UTC
Posted on October 23, 2017 at 12:20

Search the web for 'STM8L001'; you'll find a first mention of such a device in a ST presentation from 2012, and current information from this month that such a device will probably be released by the end of this year.

Philipp

S.Ma
Principal
Oct 29, 2017 2:21 PM UTC
Philipp Krause
Senior II
Oct 30, 2017 10:54 AM UTC
Posted on October 30, 2017 at 11:54

Raisonance released RKit-STM8 v1.66.17.0191 today.

One of the new features is STM8L001 support.

Philipp

Szymon PANECKI
Senior III
Dec 10, 2017 9:32 PM UTC
Posted on December 10, 2017 at 22:32

Hello,

ST has just introduced new 8-pin STM8 MCU. This is low-power STM8L001J3 device. For more information please refer to the

http://www.st.com/content/st_com/en/products/microcontrollers/stm8-8-bit-mcus/stm8l-series/stm8l-value-line/stm8l001j3.html

.

Regards

Szymon