Skip to main content
SKaru.5
Associate
December 17, 2021
Question

any inbuild NFC , BLE and Wifi Available in STM32 Controller ?

any inbuild NFC , BLE and Wifi Available in STM32 Controller . or NFC and BLE like that any combination is available ? Please suggest the MCU .

This topic has been closed for replies.

3 replies

Peter BENSCH
ST Technical Moderator
December 17, 2021

Welcome, @SKaru.5​, to the community!

There are currently several STM32 with built-in BLE, also a ready-to-use module including an antenna.

Currently an external module is required for NFC because there are too many combinations that, depending on the function, also have to provide high transmission power.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Guillaume K
ST Employee
December 17, 2021

for BLE: STM32WB

SKaru.5
SKaru.5Author
Associate
December 18, 2021

Thanks for your Reply.

if we select STM32WB for BLE and for NFC Interface any Evaluation Board is available .

NFC - P2P and Reader/Write Mode