Skip to main content
darkore
Associate II
Nov 1, 2008 5:21 PM UTC
Question

[ANN] eLua (Lua for microcontrollers) 0.5 released

Posted on November 01, 2008 at 18:21

[ANN] eLua (Lua for microcontrollers) 0.5 released

This topic has been closed for replies.

1 reply

darkore
darkoreAuthor
Associate II
May 17, 2011 7:56 AM UTC
Posted on May 17, 2011 at 09:56

Hi,

eLua is an open source effort to bring the Lua programming language in the embedded world (MCUs). It is meant to be a complete MCU development environment. It currently runs on a number of ARM variants (STR912FAW44 included), as well as Cortex (and i386 as a proof of concept). Version 0.5 was just released, this is the changelog:

* Added support for STR7 CPUs from ST

* Added TCP/IP support using the uIP stack

* Added support for console and shell over TCP/IP instead of serial link

* Added the ''net'' module (eLua's interface to TCP/IP functions)

* Added the ''cpu'' module (eLua's interface to the target CPU)

* New samples: morse.lua (Morse code encoder), lhttpd.lua (Lua scripting HTTP server)

* Added support for cross-compiling Lua code (compile on PC, run on target)

* XMODEM can now receive Lua bytecode in addition to Lua source code

* The XMODEM buffer is now dynamic (grows as needed) instead of fixed size

* Project documentation updated

For more details visit the project web page at

http://elua.berlios.de

Best,

Bogdan