Skip to main content
Associate III
March 31, 2024
Question

AN2659, chaining interrupts, how?

AN2659, section 4.1.3 Vector table redirection, says that "The primary interrupt table contains a set of jumps to the user interrupt table" but the same code that accompanies this document does not seem to implement this - does this code just need to be extended?

Also AN2659 claims that if I edit the USER BOOTLOADER PROTOCOL PARAMETERS etc in `main.h` then the resulting code will use these but this does not seem to be correct.  For example the pin that triggers the bootloader appears to be hardcoded to GPIOD and ignores the user custom settings.  Did I miss something?

    This topic has been closed for replies.

    1 reply

    Associate III
    April 5, 2024

    This is how I have created the bootloader vector table, which I think should chain to my application which starts at flash address 0x8A00 (the application vector table is at that address).  Is this the way I should be doing this?

    #define MAIN_USER_RESET_ADDR 0x8A00ul
    
    struct interrupt_vector const _vectab[] = {
    	{0x82, (interrupt_handler_t)_stext}, /* reset */
    	{0x82, NonHandledInterrupt}, /* trap */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+8)}, /* irq0 */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+12)}, /* irq1 */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+16)}, /* irq2, CLK */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+20)}, /* irq3, EXTI0 */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+24)}, /* irq4, EXTI1 */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+28)}, /* irq5, EXTI2 */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+32)}, /* irq6, EXTI3 */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+36)}, /* irq7, EXTI4 */
    	{0x82, NonHandledInterrupt}, /* irq8, reserved */
    	{0x82, NonHandledInterrupt}, /* irq9, reserved */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+48)}, /* irq10, SPI, end of transfer */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+52)}, /* irq11, TIM1 */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+56)}, /* irq12, TIM1 */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+60)}, /* irq13, TIM2 */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+64)}, /* irq14, TIM2 */
    	{0x82, NonHandledInterrupt}, /* irq15, reserved */
    	{0x82, NonHandledInterrupt}, /* irq16, reserved */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+76)}, /* irq17, UART1, Tx complete */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+80)}, /* irq18, UART1, Receive register DATA FULL */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+84)}, /* irq19, I2C */
    	{0x82, NonHandledInterrupt}, /* irq20, reserved */
    	{0x82, NonHandledInterrupt}, /* irq21, reserved */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+96)}, /* irq22, ADC1 */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+100)}, /* irq23, TIM4 */
    	{0x82, (interrupt_handler_t)(MAIN_USER_RESET_ADDR+104)}, /* irq24, flash */
    	{0x82, NonHandledInterrupt}, /* irq25, reserved */
    	{0x82, NonHandledInterrupt}, /* irq26, reserved */
    	{0x82, NonHandledInterrupt}, /* irq27, reserved */
    	{0x82, NonHandledInterrupt}, /* irq28, reserved */
    	{0x82, NonHandledInterrupt}, /* irq29, reserved */
    };

    .