Skip to main content
giovanni239955
Associate III
April 2, 2004
Question

Alternative flash programmer for ST9

  • April 2, 2004
  • 13 replies
  • 2305 views
Posted on April 02, 2004 at 06:22

Alternative flash programmer for ST9

This topic has been closed for replies.

13 replies

bertrand23
Visitor II
May 17, 2011
Posted on May 17, 2011 at 11:34

What about the Segger Flasher. It should be optimized for Volume Production.

giovanni239955
Associate III
May 17, 2011
Posted on May 17, 2011 at 11:34

Hi, anyone can suggest a faster (than STVP) flash programmer for ISP programming of ST92F150?

Thanks

bertrand23
Visitor II
May 17, 2011
Posted on May 17, 2011 at 11:34

Do you belong to a company involved with Devt Tools or did you design this programmer to solve your own application problem.

siegmund
Associate III
May 17, 2011
Posted on May 17, 2011 at 11:34

we developed this tool cause the ST-programming board is not usable for production und the segger tool is too unflexible.

we had another small application, so it was no long way to redesign it as a ISP-Tool for the ST9.

It generates the RESET und other ISP-Signals and transfers data from/to the PC via RS232.

The PC kann interoperate with a simple script file or manual actions do perform actions:

reset

erase flash sector

erase chipflash

donwload hexfile

download binfile

load your application into ram and execute it

the last point is remarkable: you can execute applications without the need of programming the flash! so you are able to test special functions very fast.

the tool is connected the the target-system with the 6 lines:

+5V/GND/RESET and the ISP-Signals.

regards,

siggi
bertrand23
Visitor II
May 17, 2011
Posted on May 17, 2011 at 11:34

Sure, can you tell us more about your tool, how you came to develop it?

siegmund
Associate III
May 17, 2011
Posted on May 17, 2011 at 11:34

hi!

we developed a small and flexible in-system-programming-box, which allows to programm the ST9x devices.

Simply connected to PC via RS232, it is possible to run scripts for predefined actions, i.e. RESET, FLASH-ERASE, PROGRAMM, LOAD-BOOT-APPLICATION, ...

even it is possible to run own small programms in the internal RAM without programming the flash!

is anyone interested?

email me.

regards, siggi
lchossat29
Visitor II
May 17, 2011
Posted on May 17, 2011 at 11:34

Hi siggi

Your tool looks good! If you use ISP, you probably need HW between your application and PC? Is it working as the ST programming board? I mean with another micro as a master...?

siegmund
Associate III
May 17, 2011
Posted on May 17, 2011 at 11:34

we designed the tool to get best results for development AND production-use.

as mentioned earlier, it is very flexible and therfore for many tasks useful.
siegmund
Associate III
May 17, 2011
Posted on May 17, 2011 at 11:34

hi

if anybody is still interested, please feel free to send me a message.
bertrand23
Visitor II
May 17, 2011
Posted on May 17, 2011 at 11:34

Hello Siggi,

We tried to contact you directly few weeks ago, but apparantly did not succeed to reach you. We are still interested by getting information on your Programmer. Could you please send us your email via the Contact Us screen on stmcu.com home page.

Bye.

arnie