Skip to main content
gtrotter
Visitor II
Aug 21, 2014 7:18 PM UTC
Question

ADC1 with with COMP1?

Posted on August 21, 2014 at 21:18

Hello,

I am working on an application which requires the use of the ADC1 peripheral as well as the COMP1 & COMP2 peripherals. There does not appear to be anything in the datasheet against this, but there is a note in the comparator driver:

''COMP1 comparator and ADC can't be used at the same time since they share the same ADC switch matrix (analog switches).''  -stm8l15x_comp.c

Is this a limitation of the driver, or of the chip? If it is a chip limitation, could someone please point me in the direction of the datasheet that mentions it? If it is a driver limitation, does anyone know if there is there a work-around?

Thanks!

Gabrielle
    This topic has been closed for replies.